Skip to main content
Associate III
Jul 11, 2025 2:02 PM UTC
Question

UART reception error

Hello,

I am using Nucleo f446re board to interface with a sensor over UART. sensor is able to send the response data frame  over rx line to mcu as mcu sends uart frame.

This transaction or data transfer is visually verified using logic analyser.

Actual issue is stm 32 is not able to capture the response packet.

Could you please assist to fix it.

Sensor sends 3 byte response frame.  0x08-0x00-0x0A 

But mcu reads it as 0x00-0x08-0x00

Let me know if you need more information.

if (HAL_UART_Transmit (dev->uartHandle, (const uint8_t *)&txReadBuff, sizeof (txReadBuff), 5)!=HAL_OK)
 return HAL ERROR:

if (HAL_UART_Receive (dev->uartHandle, (uint8_t *) &ackBuff, sizeof(ackBuff), 5)!=HAL_OK)
 return HAL ERROR

 

AckBuff is an array of 3 bytes / uint8_t type.


Edited to apply source code formatting - please see How to insert source code for future reference.

This topic has been closed for replies.

6 replies

Andrew Neil
Super User
Jul 11, 2025 2:12 PM UTC

Please show the full code - or, preferably, a minimum but complete example which illustrates the problem.

Have you checked the UART error flags to see if any errors are occurring (Framing, etc) ?

It looks like your code is not ready when the sensor starts sending

Have you tested your code using a terminal - before adding the extra uncertainties of the sensor?

Does the sensor have a protocol with defined frame structure? If so, better to receive under interrupt and parse that structure rather than just wait for an arbitrary number of characters with no synchronisation...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
Jul 11, 2025 2:16 PM UTC

This is actually happening while reading one particular register.samw function works fine for rad action on other 

 

Karl Yamashita
Principal
Jul 12, 2025 1:07 AM UTC

The HAL_UART_Receive may not be ready by the time you call it. Use UART Rx interrupt instead so that it's always ready to receive even before HAL_UART_Transmit returns from it's call. 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Chaima_M
ST Employee
Jul 14, 2025 11:17 AM UTC

Hello @Alex_reynold ,

This issue can occur due to noise on the RX line, so please ensure that no noise is present on the RX line. 

With best regards.

Associate III
Jul 14, 2025 12:41 PM UTC

Any suggestions to reduce the noise

Andrew Neil
Super User
Jul 14, 2025 12:59 PM UTC

Check first if you do actually have noise!

Look at the signals using an oscilloscope ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.