Skip to main content
Associate III
Nov 12, 2025 3:25 PM UTC
Question

Trying to receive CAN PDO( RPDO) with STM32C02RC , canopenSTM32 and CanopenEditor

Hello everyone,

I’m currently facing an issue with PDO data exchange between a CANopen Master and Slave running on STM32 using CanopenSTM32 and CANopenEditor.

I can successfully see PDO frames on the CAN bus using a Waveshare USB-CAN-FD analyzer, but my Slave does not seem to receive or update the mapped object as expected.
These are the Details of my Setup: 

  • Master Node-ID: 0x18

  • Slave Node-ID: 0x02

  • Stack: CANopenNode V4 (ported for STM32)

  • ODs generated with: CANopenEditor v4.2.3

  • Bus monitoring tool: Waveshare USB-CAN-FD

     

    Master TPDO1 (0x1800): 

COB-IDUsedByTPDO = 0x40000180
Mapping = 0x60010020 (x6001_counter)
TransmissionType = 0xFF

So, on the CAN bus, the Master sends messages with ID: 0x180 + Node-ID = 0x180 + 0x18 = 0x198. And I can confirm this with my USB-CAN-FD analyzer i  see CAN frames with ID 0x198 and correct payload.


Slave RPDO1 (0x1400): 

COB-IDUsedByRPDO = 0x40000180 <-- initially
Mapping = 0x60020020 (x6002_counterFromH7)
TransmissionType = 0xFF


So the Slave was originally listening on 0x180, but the Master sends on 0x198.
but i changed  the RPDO COB-ID in the Slave OD to 0x40000198.


And On my Master :   i am just sending through the network, which is also visible with my Analyser.

 
OD_PERSIST_COMM.x6001_counter ++ ;

 CO_TPDOsendRequest(&canopenNodeSTM32->canOpenStack->TPDO[0]);

 HAL_Delay(1000);



However, no matter what I change in the Slave configuration,
the received value always stays 0 (default).

CO_process_RPDO(CO, false);
printf("Received: %lu\n", (unsigned long)OD_PERSIST_COMM.x6002_counterFromH7);

Has anyone experienced a similar issue where PDO messages appear correctly on the CAN bus, but the Slave’s mapped variable never updates?
Is there anything else I should check — such as modifying the COB-ID or whatever? 

1 reply

MHoll.2
Senior III
Nov 12, 2025 3:52 PM UTC

This is a Canopen Stack specific question, probably better to ask on the CanOpenNode forum (https://sourceforge.net/p/canopennode/discussion/387151/).

Normaly the Master has to send the PDO's with the COB-ID of the slave (in your case 0x182).

If You have modifed the COB-ID directly in the CanOpenEditor, the probably the slave is now expecting COB-ID 0x198 + 0x02 = 0x19A.