Skip to main content
fbackvid
Associate
Nov 17, 2019 11:28 AM UTC
Question

Truestudio was working fine. After adding 1 line in a source file, I got stuck with the attached error message. Changing the source back to original did not help, still getting the same error. Any suggestions how to proceed?

No source file named C:\\vmi\\viber_x4\\x4_fw_1_1\\BootLoader\\SRC\\bl_main.c.

Program received signal SIGTRAP, Trace/breakpoint trap.

GR_IconMenu (iconSTR=0x23a0008, Options=0) at ..\..\COMMON\SRC\GraphMenus.c:151

151    if (xCount == 0)

Halted to watchpoint

Core context saved

Load the program in memory

Loading section .fastcode, size 0x7050 lma 0x0

Loading section .isr_vector, size 0x298 lma 0x20000000

Loading section .fastdata, size 0xc0 lma 0x20000298

Loading section .text, size 0x49f90 lma 0x70000000

Loading section .ARM, size 0x8 lma 0x70049f90

Loading section .rodata, size 0x9668 lma 0x71200000

Loading section .init_array, size 0x4 lma 0x71209668

Loading section .fini_array, size 0x4 lma 0x7120966c

Loading section .data, size 0x196c lma 0x71209670

Start address 0x70000eb0, load size 377628

Transfer rate: 96 KB/sec, 2839 bytes/write.

Program loaded

CPU context restored

 Abort any bootloader task

Temporary breakpoint 4 at 0x70027f3a: file ..\SRC\VX4_Main.c, line 126.

 Launch the program using the bootloader

$1 = 1520805210

warning: Remote failure reply: E31

/home/build/gcc-arm-none-eabi-6-2017-q1-update/src/gdb/gdb/thread.c:817: internal-error: is_thread_state: Assertion `tp' failed.

A problem internal to GDB has been detected,

further debugging may prove unreliable.

Quit this debugging session? (y or n) [answered Y; input not from terminal]

C:\Users\fb\AppData\Local\Temp\truestudio6664351465486505174gdbscript:64: Error in sourced command file:

Remote communication error. Target disconnected.: No error.

This is a bug, please report it. For instructions, see:

<http://www.gnu.org/software/gdb/bugs/>.

/home/build/gcc-arm-none-eabi-6-2017-q1-update/src/gdb/gdb/thread.c:817: internal-error: is_thread_state: Assertion `tp' failed.

A problem internal to GDB has been detected,

further debugging may prove unreliable.

Create a core file of GDB? (y or n) [answered Y; input not from terminal]

This topic has been closed for replies.