Skip to main content
NWADE.1
Associate
Sep 25, 2020 3:03 PM UTC
Question

TCP/IP - STM32F767ZI-Nucleo - Cannot manage to make it work - ETH

Hello,

Today and for the past days I am struggling trying to setup a TCP/IP server on the STM32F767Zi-Nucleo board..

The IP address is set to :

192.168.0.10

The mast address is set to :

255.255.255.0

The gateway address is set to :

192.168.0.1

My local machine show an IP address : 192.168.1.95

From my PC I am able to ping the board (w/ delay ~.025ms)

The main function is defined as :

int main(void)
{
 HAL_Init();
 
 SystemClock_Config();
 
 MX_GPIO_Init();
 osKernelInitialize();
 
 defaultTaskHandle = osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes);
 osKernelStart();
 
 while (1)
 {
 }
}

The task is defined as :

void StartDefaultTask(void *argument)
{
 MX_LWIP_Init();
 printf("Entered task\n");
 tcp_echoserver_init();
 
 for(;;)
 {
 
 }
}

And the server initialization :

void tcp_echoserver_init(void) {
	local = netconn_new(NETCONN_TCP);
	if (local == NULL) {
		printf("Setup local connection failed\n");
		return;
	}
	printf("Local connection initialized\n");
	err_t err;
 
	err = netconn_bind(local, IP_ADDR_ANY, 7); // open port 7 || WILL BE CHANGED
 
	struct netbuf *buf = netbuf_new();
	void *data;
	uint16_t len;
 
	if (err == ERR_OK) {
		printf("Connection binded to port 7\n");
		err = netconn_listen(local); // set listening mode
		if (err != ERR_OK) printf("listen issue\n");
		printf("Port 7 is in listening mode\n");
		printf("Socket : %d\n", local->socket); // -1 is a problem
		while (1) {
			printf("Accepting..\n");
			err = netconn_accept(local, &remote);
			if (err == ERR_OK) {
				printf("Accepted!\n");
				while ((err = netconn_recv(remote, &buf)) == ERR_OK) {
					do {
						netbuf_data(buf, &data, &len);
						netconn_write(remote, data, len, NETCONN_COPY);
					} while (netbuf_next(buf) >= 0);
					netbuf_delete(buf);
				}
				netconn_close(remote);
				netconn_delete(remote);
			}
		}
	} else {
		printf("Bind issue\n");
		netconn_delete(remote);
	}
}

In my ioc file the clock is configured : 0693W000004H9cJQAS.png

I didn’t showed the rest since only this part is manually configurable.

LWIP Config :

Version 2.12 and DHCP disabled

0693W000004H9cTQAS.png

The rest is at default configuration

I also turned on RTOS :

API : CMSIS v2

FreeRTOS version 10.2.1

CMSIS-RTOS 2.0

The ETH port is enabled in RMII with global interrupt (w/o wake-up interrupt EXTI line 19)

RCC is Crystal/Ceramic Resonator HSE, rest of configuration unchanged

And SYS :

Debug to Serial Wire with timebase source TIM1 (as RTOS wont use Systick)

When launching debug session I got the following output in ITM console I got the following output :

Entered task
Local connection initialized
Connection binded to port 7
Port 7 is in listening mode
Socket : -1
Accepting..

For output to work. change write function from

__attribute__((weak))
int _write(int file, char *ptr, int len)
{
	int DataIdx;
 
	for (DataIdx = 0; DataIdx < len; DataIdx++)
	{
		__io_putchar(*ptr++);
	}
	return len;
}

to

//__attribute__((weak))
int _write(int file, char *ptr, int len)
{
	/* Implement your write code here, this is used by puts and printf for example */
	for(int i = 0 ; i < len ; i++) ITM_SendChar((*ptr++));
	return len;
//	int DataIdx;
//
//	for (DataIdx = 0; DataIdx < len; DataIdx++)
//	{
//		__io_putchar(*ptr++);
//	}
//	return len;
}

From there I simply though : “Hey let’s use netcat or whatever and just connect.�?

0693W000004H9dbQAC.png

Or setting a C project that going to communicate with the board (as it is my final goal)

client.c

#include <netdb.h> 
#include <stdio.h> 
#include <stdlib.h> 
#include <string.h> 
#include <sys/socket.h> 
#include <unistd.h>
#include <arpa/inet.h>
 
#define MAX 80 
#define PORT 8080 
#define SA struct sockaddr 
void func(int sockfd) 
{ 
 char buff[MAX]; 
 int n; 
 for (;;) { 
 bzero(buff, sizeof(buff)); 
 printf("Enter the string : "); 
 n = 0; 
 while ((buff[n++] = getchar()) != '\n') 
 ; 
 write(sockfd, buff, sizeof(buff)); 
 bzero(buff, sizeof(buff)); 
 read(sockfd, buff, sizeof(buff)); 
 printf("From Server : %s", buff); 
 if ((strncmp(buff, "exit", 4)) == 0) { 
 printf("Client Exit...\n"); 
 break; 
 } 
 } 
} 
 
int main() 
{ 
 int sockfd, connfd; 
 struct sockaddr_in servaddr, cli; 
 
 // socket create and varification 
 sockfd = socket(AF_INET, SOCK_STREAM, 0); 
 if (sockfd == -1) { 
 printf("socket creation failed...\n"); 
 exit(0); 
 } 
 else
 printf("Socket successfully created..\n"); 
 bzero(&servaddr, sizeof(servaddr)); 
 
 // assign IP, PORT 
 servaddr.sin_family = AF_INET; 
 servaddr.sin_addr.s_addr = inet_addr("127.0.0.1"); 
 servaddr.sin_port = htons(PORT); 
 
 // connect the client socket to server socket 
 if (connect(sockfd, (SA*)&servaddr, sizeof(servaddr)) != 0) { 
 printf("connection with the server failed...\n"); 
 exit(0); 
 } 
 else
 printf("connected to the server..\n"); 
 
 // function for chat 
 func(sockfd); 
 
 // close the socket 
 close(sockfd); 
}

server.c

#include <stdio.h> 
#include <netdb.h> 
#include <netinet/in.h> 
#include <stdlib.h> 
#include <string.h> 
#include <sys/socket.h> 
#include <sys/types.h>
#include <unistd.h>
 
#define MAX 80 
#define PORT 8080 
#define SA struct sockaddr 
 
// Function designed for chat between client and server. 
void func(int sockfd) 
{ 
 char buff[MAX]; 
 int n; 
 // infinite loop for chat 
 for (;;) { 
 bzero(buff, MAX); 
 
 // read the message from client and copy it in buffer 
 read(sockfd, buff, sizeof(buff)); 
 // print buffer which contains the client contents 
 printf("From client: %s\t To client : ", buff); 
 bzero(buff, MAX); 
 n = 0; 
 // copy server message in the buffer 
 while ((buff[n++] = getchar()) != '\n') 
 ; 
 
 // and send that buffer to client 
 write(sockfd, buff, sizeof(buff)); 
 
 // if msg contains "Exit" then server exit and chat ended. 
 if (strncmp("exit", buff, 4) == 0) { 
 printf("Server Exit...\n"); 
 break; 
 } 
 } 
} 
 
// Driver function 
int main() 
{ 
 int sockfd, connfd, len; 
 struct sockaddr_in servaddr, cli; 
 
 // socket create and verification 
 sockfd = socket(AF_INET, SOCK_STREAM, 0); 
 if (sockfd == -1) { 
 printf("socket creation failed...\n"); 
 exit(0); 
 } 
 else
 printf("Socket successfully created..\n"); 
 bzero(&servaddr, sizeof(servaddr)); 
 
 // assign IP, PORT 
 servaddr.sin_family = AF_INET; 
 servaddr.sin_addr.s_addr = htonl(INADDR_ANY); 
 servaddr.sin_port = htons(PORT); 
 
 // Binding newly created socket to given IP and verification 
 if ((bind(sockfd, (SA*)&servaddr, sizeof(servaddr))) != 0) { 
 printf("socket bind failed...\n"); 
 exit(0); 
 } 
 else
 printf("Socket successfully binded..\n"); 
 
 // Now server is ready to listen and verification 
 if ((listen(sockfd, 5)) != 0) { 
 printf("Listen failed...\n"); 
 exit(0); 
 } 
 else
 printf("Server listening..\n"); 
 len = sizeof(cli); 
 
 // Accept the data packet from client and verification 
 connfd = accept(sockfd, (SA*)&cli, &len); 
 if (connfd < 0) { 
 printf("server acccept failed...\n"); 
 exit(0); 
 } 
 else
 printf("server acccept the client...\n"); 
 
 // Function for chatting between client and server 
 func(connfd); 
 
 // After chatting close the socket 
 close(sockfd); 
}

gcc server.c -o server && gcc client.c -o client

0693W000004H9vzQAC.png

When changing client server address fomr 127.0.01 to 192.168.0.10 and port from 8080 to 7

0693W000004H9wTQAS.png

So… PC-wise it seems to work. But the connection is never accepted on the board.

I also tried to use the project from the git :

LwIP_HTTP_Server_Netconn_RTOS under STM32CubeF7-master/Projects/STM32F767ZI-Nucleo/Applications/LwIP/LwIP_HTTP_Server_Netconn_RTOS

removed the line #define USE_LCD and #define USE_DHCP

changing the IP by the one I set on my board. Still have no result. Trying to access the webpage at 192.168.0.10:80 shows “Unable to connect�? from e.g. Firefox

I also tried to use MBED /w their IDE, still get no results.

I've only been working with STM board since like... 3-4 month on only 2projects, the one only involved USART & i2C communication (way easier). That's for my background w/ MCUs :)

Thanks a lot !

Nicolas

This topic has been closed for replies.

3 replies

Pavel A.
Sep 26, 2020 10:40 PM UTC

Is this a new from scratch project created in Cube, or adaptation of some example provided by ST in the package for this Nucleo board?

If the former - please get a ready example working on your board first.

-- pa

NWADE.1
NWADE.1Author
Associate
Sep 28, 2020 7:42 AM UTC

Hello Pavel A.

Yes, this is a project created using CubeMX IDE and I extracted the functions used in the example to try it.

As the example only use functions from the LwIP library, I reused the same code. My understanding of it is that, I missed something during the configuration of the project.

On the other hand, only using the project within the archive ( STM32CubeF7-master ) and launching it as is, doesn't work either. (as specified in the end of my post, I remove the USE_DHCP and USE_LCD define from this project. Since I do not use them.

Also trying a simple program using Mbed Studio (on the same board)

#include "mbed.h"
#include "EthernetInterface.h"
 
// Network interface
EthernetInterface net;
 
// Socket demo
int main()
{
 // Bring up the ethernet interface
 printf("Ethernet socket example\n");
 net.connect();
 
 // Show the network address
 SocketAddress a;
 net.get_ip_address(&a);
 printf("IP address: %s\n", a.get_ip_address() ? a.get_ip_address() : "None");
 
 // Open a socket on the network interface, and create a TCP connection to mbed.org
 TCPSocket socket;
 socket.open(&net);
 
 net.gethostbyname("ifconfig.io", &a);
 a.set_port(80);
 socket.connect(a);
 // Send a simple http request
 char sbuffer[] = "GET / HTTP/1.1\r\nHost: ifconfig.io\r\n\r\n";
 int scount = socket.send(sbuffer, sizeof sbuffer);
 printf("sent %d [%.*s]\n", scount, strstr(sbuffer, "\r\n") - sbuffer, sbuffer);
 
 // Recieve a simple http response and print out the response line
 char rbuffer[64];
 int rcount = socket.recv(rbuffer, sizeof rbuffer);
 printf("recv %d [%.*s]\n", rcount, strstr(rbuffer, "\r\n") - rbuffer, rbuffer);
 
 // Close the socket to return its memory and bring down the network interface
 socket.close();
 
 // Bring down the ethernet interface
 net.disconnect();
 printf("Done\n");
}

Return the following result.

IP address: None

sent -3004 [GET / HTTP/1.1]

-3304 == NSAPI_ERROR_NO_CONNECTION

Meaning I'm not connected to a network.

Edit : The thing is I cannot manage to have an example working.

wastl
Associate
Jan 7, 2021 9:12 PM UTC

Dear all,

I have the same problem, I am not able to manage getting the "LwIP_HTTP_Server_Netconn_RTOS" example run.

I am using STM32CubeIDE (version 1.5.1), imported the example, but when I try to build the application, errors occur with files missing (e.g. httpd_opts.h which should be located in directory "lwip/apps"). There problem is, that the missing files are not part of the imported project (they are not there on disk).

Is there anybody who got this example running on the STM32F767Zi-Nucleo board using the STM32CubeIDE?

Kind regards.