Skip to main content
kent gu
Associate III
Dec 1, 2017 3:30 AM UTC
Solved

SW enter HardFault_Handler using OpenStm32

Posted on December 01, 2017 at 04:30

Hi,

The project is developed with Keil MDK, it run well. But I use OpenStm32 to create one project, and copy the source code into the OpenStm32 project. I can run with ST Jlink V2, but the code enter HardFault_Handler while run ''TIM_Cmd(TIM4,ENABLE); ''. 

BTW, I use old stm32f10x_it.c (V3.3.0) version?other driver file are old version.

0690X00000604HZQAY.jpg

Best Regards,

Kent

#openstm32-debug #driver-version
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 1, 2017 3:57 AM UTC
Posted on December 01, 2017 at 04:57

Need to make sure you have a TIM4 IRQ Handler set up.

Check also the reason of the Hard Fault, having it as a while(1) loop isn't very enlightening.

Check also for uninitialized pointers, or code in the TIM4_IRQHandler that does a division, this can trap if you divide by zero, so check before doing the math.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 1, 2017 3:57 AM UTC
Posted on December 01, 2017 at 04:57

Need to make sure you have a TIM4 IRQ Handler set up.

Check also the reason of the Hard Fault, having it as a while(1) loop isn't very enlightening.

Check also for uninitialized pointers, or code in the TIM4_IRQHandler that does a division, this can trap if you divide by zero, so check before doing the math.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
kent gu
kent guAuthor
Associate III
Dec 1, 2017 6:40 AM UTC
Posted on December 01, 2017 at 06:40

Clive,

Thank you a lot for your reminder. Yes, seems that I import wrong startup file, which not include Tim4  vector. I solved the problem with the correct startup file.

Best Regards,

Kent