Skip to main content
JMazu.1
Associate III
Dec 27, 2023 5:51 AM UTC
Solved

STSW-EDUKIT: How can I view the sprintf messages.

Hi Folks,

Managed to get the source compiled and loaded for the inverted pendulum project.  Rather impressive.

In the source code there's sprintf statements to inform the user on what's going on.

My question is: How can I view these messages?

I'm a bit rusty with STF401 code, just forgotten how to do things.

Can someone please help me?

Thanks,
John.

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
Jan 4, 2024 5:58 PM UTC

--- most times : 115200 --- but just look in the source (UART2 setting, in MX_UART2_init), you said, you have it. I dont.

+

in my ide 1.13.1 , it was there ... afair. But not sure about this. :)

 

 

If you feel a post has answered your question, please click on " Best Answer ".

13 replies

JMazu.1
JMazu.1Author
Associate III
Jan 1, 2024 1:47 PM UTC

Hi,

Still stuck.

The project is peppered with sprintf commands, however I have no idea how to view these messages.

I'm assuming I have to run in Debug mode.

What do I have to do to view these messages?

Thanks,
John.

JMazu.1
JMazu.1Author
Associate III
Jan 2, 2024 1:55 PM UTC

Hi,

Can someone please help me?

Thanks,
John.

JMazu.1
JMazu.1Author
Associate III
Jan 2, 2024 2:26 PM UTC

Hi,

I've searched the Internet and unfortunately they all use ioc as a stepping stone.

With the STSW-EDUKIT project everything is done in code, the long way.  No ioc.
The main.c file is over 6,000 lines long.  Everything is in main.c.

Surely there must be some way to view these sprintf messages in some  sort of a console.

I'll keep looking, but don't be shy if you know the answer.

Thanks,
John.

AScha.3
Super User
Jan 2, 2024 2:42 PM UTC

Hi,

I dont have the source - so what should i say about ? :)

Maybe you attach a xx.zip ...

If you feel a post has answered your question, please click on " Best Answer ".
JMazu.1
JMazu.1Author
Associate III
Jan 4, 2024 2:36 AM UTC

Thanks AScha.3,

I'll have a look into it.

JMazu.1
JMazu.1Author
Associate III
Jan 4, 2024 9:38 AM UTC

Just a bit of background AScha.3,

In Arduino Land, the message is sent via Serial.print.
In the Arduino IDE, you select which port to use and that's it, everything appears in the console.

I was hoping for something similar with the STMCubeIDE environment.
Wishful thinking eh?

AScha.3
Super User
Jan 4, 2024 10:01 AM UTC

No - just try it :

in IDE , bottom window : console view

AScha3_0-1704362193388.png

click on -> small dropdown arrow , right -> command shell console

you get :

AScha3_1-1704362335966.png

first time : -> New ....then choose the USB-serial (on your system maybe COM9 or...)

and you are there.... :)

(next time : name field should show your already made connections )

IDE (eclipse) is very powerful - just the problem is: how to find or set , what you want (not only for you, same for me...).

Then looks like this - when connected:

AScha3_2-1704362844917.png

 

If you feel a post has answered your question, please click on " Best Answer ".
JMazu.1
JMazu.1Author
Associate III
Jan 4, 2024 5:52 PM UTC

Thanks ASsch.3.

The STM32CubeIDE is a most complex piece of software.  The terminal is NOT part of the original download, you need to download is a separate step.

I can now start a terminal session but alas I haven't worked out what the Baud Rate is.  All I get displayed are random characters but at least that's something.

I will keep trying.

AScha.3
AScha.3Best answer
Super User
Jan 4, 2024 5:58 PM UTC

--- most times : 115200 --- but just look in the source (UART2 setting, in MX_UART2_init), you said, you have it. I dont.

+

in my ide 1.13.1 , it was there ... afair. But not sure about this. :)

 

 

If you feel a post has answered your question, please click on " Best Answer ".
JMazu.1
JMazu.1Author
Associate III
Jan 5, 2024 3:46 AM UTC

Hi AScha.3,

Good news, I checked the huart2 structure and found the baud rate was  set 230,400, not quite a standard rate and very fast.

I found a declaration of SAMPLE_BAUD_RATE = 230400.
I changed it 9,600 baud and all works well.

Thanks for your assistance in solving this problem.