Skip to main content
MRuhe.1
Associate II
Jun 26, 2025 4:58 PM UTC
Question

STM32U585VIT6 Programming Error

Hi All,

I am choose the STM32U585VIT6 MPU to design our customized board. Firstly I design a simple basic connection to program it and only blink the LED for confirmation our initially circuit. Also I following the  AN5373 document.

When I flash the code getting the error below

Error in initializing ST-LINK device.

Reason : No device found on target. 

Find the attached schematic.

Please guide me what is the issue and how to resolve it.

10 replies

TDK
Jun 26, 2025 6:03 PM UTC

Is the chip powered?

Try to connect with STM32CubeProgrammer. If unsuccessful, show a screenshot.

Schematic looks fine.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
MRuhe.1
MRuhe.1Author
Associate II
Jun 27, 2025 9:33 AM UTC

Hi,

Yes chip is powered 3V3 externally and all the ground are common. I already try many times to program the chip using ST-LINK V2 and ST-LINK V2 IOSL but getting the same error shown in shared image.

Also I shared screenshot.

Thanks.

Tesla DeLorean
Guru
Jun 27, 2025 3:32 AM UTC

It's an MCU, not an MPU, like an embedded Linux STM32MP device.

ST-LINK reports voltage correctly, Pin 1 or 2 should be VTarget for the pin drivers to work.

Check with STM32 Cube Programmer 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MRuhe.1
MRuhe.1Author
Associate II
Dec 8, 2025 1:07 PM UTC

Thanks to all. The issue is resolved.

ST Technical Moderator
Dec 8, 2025 4:25 PM UTC

Hi @MRuhe.1 

Glad to know the issue has been solved.

Please close this thread by marking the helpful reply as "Accept as Solution". This will help other community members with the same issue to find the answer faster.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks