Skip to main content
Associate III
Jun 16, 2025 5:13 PM UTC
Question

STM32N65 DK - alternative for DDRAM APS256XXN-OBR-BG

Hello All,

I'm working on a board, wherein i am using DRAM 256Mb 200MHz with Mfr. No: part no   APS256XXN-OBR-BG (as recommended in STM32N65 DK) but while going through it i found that this part no is not recommended for the new design. Can anyone please share the alternative of this part no or guide in this.

 

 

sakshi_0-1750093769270.png

 

Best Regards,

Sakshi 

 

 

5 replies

KDJEM.1
ST Technical Moderator
Jul 8, 2025 10:27 AM UTC

Hello @sakshi;

 

As mentioned in AN5050 section "10 Supported device", the Octo-SPI, Hexadeca-SPI, and XSPI interface can operate in two different low-level protocols: Regular-command and HyperBus.

  • Thanks to the regular-command frame format flexibility, any Single-SPI, Dual-SPI, Quad-SPI, or Octo-SPI or 16-bit memory can be connected to an STM32 device. There are several suppliers of Octo-SPI or 16-bit compatible memories (such as Macronix, Adesto, Micron, AP Memory, Infineon, or Winbond).
  • Thanks to the HyperBus protocol support, several HyperRAM, and HyperFlash™ memories are supported by the STM32 devices. Some memory manufacturers (such as Infineon, Winbond, or ISSI) provide HyperRAM and HyperFlash™ memories.

Also, I recommend you to verify that the command format and order shared in the memory datasheet must be aligned with the command format and order for the XSPI interface mentioned in the STM32 reference.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
sakshiAuthor
Associate III
Jul 16, 2025 4:32 PM UTC

Hello @KDJEM.1 

 

Thanks for sharing the information.

Yes, I'm referring to the data sheet aswell.

 

Best Regards,

Sakshi 

MHoll.2
Senior III
Jul 8, 2025 11:09 AM UTC

Reading the description the suggested alternative is the APS256XXN-OB9-BG.

sakshiAuthor
Associate III
Jul 16, 2025 4:33 PM UTC

Hi @MHoll.2 

 

Thanks for the reply.

 

Best Regards,

Sakshi 

Will_Robertson
Associate III
Jan 5, 2026 3:29 PM UTC

Hi @sakshi @MHoll.2 and @KDJEM.1 ,

Thank you very much for this discussion - it's very valuable to read your recommendations and your explaination of the Octo-SPI, Hexadeca-SPI, and XSPI interface and the Regular-command and HyperBus protocols.

Will