Skip to main content
asighinolfi9
Associate
July 8, 2013
Question

STM32L15x: Read previously saved data in internal EEPROM

  • July 8, 2013
  • 5 replies
  • 1452 views
Posted on July 08, 2013 at 11:56

Good morning,

I need to manage the internal EEPROM of the STM32L151C6: i found some library function for erasing and programming (DATA_EEPROM_ProgramByte, etc..), but I was not able to find some function for Reading from the EEPROM the previous stored data.

If someone have had the same issue, could give me some advices?

Thank you in advance!

Andrea

#stm32l #eeprom #eeprom-rww
This topic has been closed for replies.

5 replies

mk299
Associate III
July 8, 2013
Posted on July 08, 2013 at 12:39

You can directly read from the corresponding address, e.g.

#define SRC_ADDR 0x08080000   memcpy

(&dest, (

void

*) SRC_ADDR,

sizeof

(dest));

Tesla DeLorean
Guru
July 8, 2013
Posted on July 08, 2013 at 13:21

It should read just like any other memory within the address space, like RAM, ROM, FLASH

#define SRC_ADDR 0x08080000

uint32_t *mem = (uint32_t *)SRC_ADDR; // Or set a pointer to it, could be a structure

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
asighinolfi9
Associate
July 8, 2013
Posted on July 08, 2013 at 14:05

thank you clive1 and kipp.michael, i'm trying!

kevinliao
Associate II
June 26, 2015
Posted on June 26, 2015 at 04:38

Would you please tell me how to write data into the internal EEPROM of stm32L152?

Thank you for answer.

Kevin
Tesla DeLorean
Guru
June 26, 2015
Posted on June 26, 2015 at 05:43

Review the example code

STM32L1xx_StdPeriph_Lib_V1.3.0\Project\STM32L1xx_StdPeriph_Examples\FLASH\Data_Program\main.c

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..