Skip to main content
psain.1
Associate III
Jun 3, 2025 5:35 AM UTC
Question

STM32H753IITx + OV5640 + W9812G6KH-6 + SD Card on SPI

Hi,

I have STM32H753IITx + OV5640 + W9812G6KH-6 + SD Card on SPI,  on a self made custom board.
I objective is to capture static image with camera and store it on a SD card. I have tested this setup in three situations:


1. By not using Ext RAM and using small resolution to fit the image in internal RAM, this setup works fine and i am able to write the image to SD card. 

2. Writing some data manually on Ext RAM which looks fine on memory monitor window.

3. When i try to use the Ext RAM with DCMI, some data gets written to Ext RAM but code never finds the jpeg start bytes i.e FF D9. Going step by step so i have kept everything else same even the resolution.

This is how buffers are defined:

Internal RAM: 

__attribute__((section(".ram_d1"))) uint8_t jpeg_data_buf[JPEG_BUF_SIZE_MAX]; // Store internal ram

External RAM:

__attribute__((section(".sdram_data"))) uint8_t jpeg_data_buf[JPEG_BUF_SIZE_MAX]; // Store ext ram

 

Flash.ld file snip: (Modified)

.sdram_data(NOLOAD) :

{

. = ALIGN(32);       // tried  = ALIGN(4);  also

_ssdram_data = .; /* Start of SDRAM data */

*(.sdram_data .sdram_data.*) /* Place all variables marked with .sdram_data */

. = ALIGN(32);

_esdram_data = .; /* End of SDRAM data */

} >SDRAM

 

Original:

.sdram_data:

{

. = ALIGN(4);

_ssdram_data = .; /* Start of SDRAM data */

*(.sdram_data .sdram_data.*) /* Place all variables marked with .sdram_data */

. = ALIGN(4);

_esdram_data = .; /* End of SDRAM data */

} >SDRAM AT> FLASH

 

 

other images are attached for the referenceCLOCK SETTINGS.jpgDCMI SETTINGS 2.jpgDCMI SETTINGS 1.jpgFMC SETTINGS.jpg

This topic has been closed for replies.

4 replies

KnarfB
Super User
Jun 3, 2025 5:53 AM UTC

I would suggest a more rigorous RAM test showing that the RAM chip correctly spans the intended address range. 

Like filling with known and/or pseudo random patterns and comparing checksums.

hth

KnarfB

psain.1
psain.1Author
Associate III
Jun 3, 2025 9:05 AM UTC

So.. my configuration and all parameters are fine its just that writing to RAM might be faulty??
And should i use crc16 during write and read and compare both cases?

 

Andrew Neil
Super User
Jun 3, 2025 9:30 AM UTC

Beware of simplistic memory tests!

This one has found errors for me which others have missed:

https://barrgroup.com/blog/fast-accurate-memory-test-code-c

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.