Skip to main content
Associate II
Sep 30, 2025 4:45 AM UTC
Question

STM32H747XIH6 DAC Issue

We used a DAC with a sample-and-hold circuit on one of our custom boards. The RC filter was not mounted; instead, the DAC output was directly connected to an SMA connector. We enabled the DAC in the firmware, and after testing, we observed a large amount of current flowing through the STM32 board. Upon inspection, we found a short between the 3.3V rail and ground on the STM32 board.

 

Please find the attachment for your reference.

4 replies

mƎALLEm
ST Technical Moderator
Sep 30, 2025 8:43 AM UTC

Hello,

which DAC instance?

R132 (0 ohm) fitted? (Short circuit on DAC1 output).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
SamudraAuthor
Associate II
Sep 30, 2025 10:06 AM UTC

Hai Sir,

DAC1_OUT1 is used. R132 is not mounted on the PCB, and the capacitor is also not mounted.

Still, we observed a short on 3V3. Can I mount R132 with a 5k resistor since it is connected to ground?

Please confirm.

 

Best regards,

Samudralankaiah.

 

 

mƎALLEm
ST Technical Moderator
Sep 30, 2025 10:46 AM UTC

Based on what you are saying now I don’t think the issue is coming from DAC1_OUT but from another stuff that I couldn’t determine based on the information you’ve provided at this stage.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.