Skip to main content
Associate
Feb 2, 2026 9:39 AM UTC
Solved

STM32H743 SPI Mode 0 issue reading ADS7066 registers

Hello,

I am having an SPI communication issue between an STM32H743BIT (SPI master) and a TI ADS7066IRTER ADC using SPI Mode 0 (CPOL=0, CPHA=0).

I write a configuration register and immediately read it back, but the read value does not match what was written. The logic analyzer shows correct MOSI data, but MISO often returns 0xFF or 0x80, and the SPI decoder reports “Settings mismatch”.

The write/read sequence is:

SPI_ADS7066_writeSingleRegister(hADS7066, GENERAL_CFG_ADDRESS, OPMODE_CFG_CLK_DIV_6);

if (SPI_ADS7066_readSingleRegister(hADS7066, GENERAL_CFG_ADDRESS) != OPMODE_CFG_CLK_DIV_6)
{
Throw(EMBL_ERROR);
}

Write and read functions used:

void SPI_ADS7066_writeSingleRegister(HANDLER hADS7066, uint8_t address, uint8_t data)
{
PSPI_ADS7066DESC pADS7066Desc = (PSPI_ADS7066DESC)hADS7066;
uint8_t dataTx[4] = {0};
uint8_t numberOfBytes = SPI_CRC_ENABLED(pADS7066Desc) ? 4 : 3;
EMBL_RETCODES ret;

dataTx[0] = OPCODE_WREG;
dataTx[1] = address;
dataTx[2] = data;
if (SPI_CRC_ENABLED(pADS7066Desc))
dataTx[3] = SPI_ADS7066_calculateCRC(dataTx, 3, 0xFF);

do {
ret = WRSPI_Transmit(pADS7066Desc->hSPI, dataTx, numberOfBytes);
} while (ret == EMBL_BUSY);
}

uint8_t SPI_ADS7066_readSingleRegister(HANDLER hADS7066, uint8_t address)
{
PSPI_ADS7066DESC pADS7066Desc = (PSPI_ADS7066DESC)hADS7066;
uint8_t dataTx[4] = {0};
uint8_t dataRx[4] = {0};
EMBL_RETCODES ret;

dataTx[0] = OPCODE_RREG;
dataTx[1] = address;
dataTx[2] = OPCODE_NULL;

do {
ret = WRSPI_Transmit(pADS7066Desc->hSPI, dataTx, 3);
} while (ret == EMBL_BUSY);

do {
ret = WRSPI_Receive(pADS7066Desc->hSPI, dataRx, 3);
} while (ret != EMBL_OK);

return dataRx[0];
}

I attach some figures showing the clock signal taken with oscilloscope and all the signals taken with logic analyser.

image (7).png

image (2).png

image (4).png

image (5).png

Rob Ashworth
Rob AshworthBest answer
Senior
Feb 2, 2026 1:08 PM UTC

I think the SPI clock speed is very low - possibly too low for this device.  I'd try and set it to 20-25MHz range - you only have 500kBit which is too slow to before the conversions get to the next sample.  

After that try and read one of the ADS7606 registers to see if it communicating ok.  There are 2 non-zero registers.  Try to read the SYSTEM STATUS register at Address 0x00, and check you get 0x81 back from the device.

The I also have a Salae Logic analyser - good kit, and handy for decoding the SPI outside of the STM environment.

RobAshworth_0-1770037455180.png

 

6 replies

mƎALLEm
ST Technical Moderator
Feb 2, 2026 9:41 AM UTC

Hello,

In next time please use </> to share a code. Please read How to write your question to maximize your chances to find a solution

I invite you to edit your post to comply with this rule.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Rob Ashworth
Senior
Feb 2, 2026 10:00 AM UTC

There seems to be an erroneous SPI clock signal in the start of transmission.

Also on the ADS7606 data sheet there is no Register with 0x04 - the smallest is 0x08.  Can you show you SPI initialisation settings.

GmampelAuthor
Associate
Feb 2, 2026 11:10 AM UTC

Hi Rob,

I think the logic analyzer is reading 0x04 because the clock starts incorrectly. What’s curious is that when I checked the oscilloscope, this erroneous behavior didn’t appear. In theory I should be sending 0x08, 0x01, 0x06 and then reading the same dares sanding first 0x10, 0x01(address), 0x00(Null). The I should receive the data on that register.

I’m attaching a figure showing my SPI initialization.

Gmampel_0-1770030343679.png

Thank you for the answer.

 

Rob Ashworth
Rob AshworthBest answer
Senior
Feb 2, 2026 1:08 PM UTC

I think the SPI clock speed is very low - possibly too low for this device.  I'd try and set it to 20-25MHz range - you only have 500kBit which is too slow to before the conversions get to the next sample.  

After that try and read one of the ADS7606 registers to see if it communicating ok.  There are 2 non-zero registers.  Try to read the SYSTEM STATUS register at Address 0x00, and check you get 0x81 back from the device.

The I also have a Salae Logic analyser - good kit, and handy for decoding the SPI outside of the STM environment.

RobAshworth_0-1770037455180.png

 

TDK
Feb 2, 2026 2:42 PM UTC

After SPI is initialized, do a single transfer with CS kept high. This will enable the peripheral and avoid the spurious pulse on SCK that you see in the logic analyzer plot.

"If you feel a post has answered your question, please click ""Accept as Solution""."