Skip to main content
Visitor II
Feb 14, 2026 6:34 AM UTC
Question

STM32H723ZGT6 K-Line fast-init works with K-line IC but not with TJA1021T/10/C/118 LIN transceiver

Hello ST Community,

I am working on K-Line communication using an STM32H723ZGT6 controller (EVK board) with a TJA1021T/10/C/118 LIN transceiver. The goal is to communicate with an ECU using  ISO-14230 K-line fast initialization.

The hardware path appears to be working correctly. We verified using an oscilloscope that:

1.TXD from STM32H723ZGT6 is switching correctly

2.LIN bus shows dominant pulses during fast-init and UART transmission

3.RXD reflects the LIN signal

4.SLP_N LOW-to-HIGH transition is implemented after power-up

NXP support confirmed that the TJA1021T transceiver operation looks correct based on the waveform captures.

However, the ECU does not respond — only the transmitted request echo is observed.

Important observations:

1.The same STM32H723ZGT6 controller, ECU, and firmware work correctly when using a dedicated K-Line transceiver IC.

2.The UART configuration is 10400 baud, 8N1, and the same firmware and fast-init implementation are used.

3.The fast-init sequence used is 300 ms HIGH, 25 ms LOW, and 25 ms HIGH.

4.The same TJA1021T/10/C/118 IC also works correctly with an ESP32-S3 controller using the same hardware connections.

Because the same firmware and timing sequence work with another K-Line IC and also with the TJA1021 when used with ESP32-S3, we are trying to understand what STM32-specific behavior could affect communication when using the TJA1021.

Could anyone advise on:

1.switching a UART TX pin between GPIO and alternate-function modes on STM32H723ZGT6

2.timing behavior when changing pin modes before UART transmission


Any guidance would be appreciated.

Thank you.


shared image (3).jfifshared image (2).jfifshared image (1).jfifhere SLP_N pin is connected to controller like gpio to handle low and high through firmware.here SLP_N pin is connected to controller like gpio to handle low and high through firmware.