Skip to main content
Visitor II
Jan 5, 2026 7:11 PM UTC
Question

STM32G071 ILI9341 SPI DMA Problem

I am working on a project that requires a 320x240 LCD panel (ILI9341).  I use a nucleo board with STM32G071RB chip. The SPI communication works fine when I use a blocking HAL_SPI_Transmit() function, but it takes a while to fill the entire screen. When I use a DMA with SPI to speed it up, all colors get distorted. 

I have tried a HAL_SPI_Transmit_DMA()  - transmit only function, and a two way HAL_SPI_TransmitReceive_DMA() function.  I tried switching from 8-bit SPI to 16-bit SPI mode for DMA transfer, but always get the same color distortion problem.

A detailed analysis revealed the core problem. While transmitting the RGB565 pixel information 'RRRRRGGGGGGBBBBB', the 16-bit data is broken into two bytes 'RRRRRGGG' and 'GGGBBBBB'. In the blocking SPI transmit function both bytes are transferred.  With any configuration SPI -DMA, the second bit gets lost.  The ILI9341 controller receives a single byte and for some reason reads it, according to ChatGPT, as RGB332 'RRRBBGGG' .  There is obvious mismatch even with the RGB332 coding, that Chat GPT failed to clearly interpret.  However, it was confirmed with numerous bit-by-bit manipulations.

I will post here just one configuration of the numerous I tried.

Here is the SPI and DMA setup. 

 /* SPI1 parameter configuration*/
 __HAL_RCC_SPI1_CLK_ENABLE();

 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_MASTER;
 hspi1.Init.Direction = SPI_DIRECTION_1LINE;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 7;
 hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;

 static void MX_DMA_Init(void)
 {

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 hdma_spi1_tx.Instance = DMA1_Channel3;
 hdma_spi1_tx.Init.Request = DMA_REQUEST_SPI1_TX;
 hdma_spi1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_spi1_tx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_spi1_tx.Init.MemInc = DMA_MINC_ENABLE; 
 hdma_spi1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
 hdma_spi1_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_spi1_tx.Init.Mode = DMA_NORMAL;
 hdma_spi1_tx.Init.Priority = DMA_PRIORITY_HIGH;

 HAL_DMA_Init(&hdma_spi1_tx);
 __HAL_LINKDMA(&hspi1, hdmatx, hdma_spi1_tx);

 /* DMA interrupt init */
 /* DMA1_Channel2_3_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);

The Fill Screen function looks like this:

// Fill entire screen with ONE variable

static uint8_t blockbuf[TFT_WIDTH * BLOCK_LINES * 2];

volatile uint8_t spi_dma_done = 0;

void ILI9341_FillScreen_Color(uint16_t color)
{
 uint16_t y = 0;

 uint8_t hi = color >> 8;
 uint8_t lo = color & 0xFF;

 /* Prepare one full block */
 for (uint32_t i = 0; i < TFT_WIDTH * BLOCK_LINES; i++)
 {
 blockbuf[2*i] = hi;
 blockbuf[2*i + 1] = lo;
 }

 while (y < TFT_HEIGHT)
 {
 uint16_t lines = BLOCK_LINES;
 if (y + lines > TFT_HEIGHT)
 lines = TFT_HEIGHT - y;

 uint32_t bytes = TFT_WIDTH * lines * 2;

 /* --- Address window (command phase) --- */
 CS_LOW();
 ILI9341_SetAddressWindow_NoCS(
 0,
 y,
 TFT_WIDTH - 1,
 y + lines - 1
 );

 /* --- Data phase --- */
 DC_DATA();

 /* Start DMA */
 HAL_SPI_Transmit_DMA(&hspi1, blockbuf, bytes);

 /* Wait for completion */
 while (HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY);
 while (SPI1->SR & SPI_SR_BSY);

 // CS_HIGH(); // CS is turned off in the callback function.

 y += lines;
 }
}


void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{
 if (hspi == &hspi1)
 {
 CS_HIGH();
 spi_dma_done = 1;
 }
}

At this moment I (and Chat GPT) have exhausted our options. Any suggestion would be greatly appreciated.

3 replies

mƎALLEm
ST Technical Moderator
Jan 7, 2026 12:07 PM UTC

Hello,

You need to probe what is going on on the SPI line (MOSI) versus what it should be seen.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Explorer
Feb 9, 2026 6:55 PM UTC

Not sure if this is relevant/correct, but shouldn't you be using the HAL_SPI_TxCpltCallback function as you're using HAL_SPI_Transmit_DMA?

gbm
Super User
Feb 10, 2026 6:36 AM UTC

Most of color display controllers require CPOL=1, CPHA=1 setting. Your code uses 0,0.

I'm not a HAL expert but this setting might also be incorrect:

hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;

 The maximum number of bytes transferred by DMA in a single run is 65535.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice