Skip to main content
FJB2069
Senior
May 6, 2025
Solved

stm32F746 Custom board, capacitive to resistive touch LCD

I got my custom stm32F746 PCB Working!  It is based on the STM32F746G-DISCO.  So, for the first revision I used the same capacitive touch lcd used on the Disco.  So that all works!  But I need a resistive lcd, so I designed in a TSC2046IPWR controller.   I just want to connect a resistive panel and get it to function.

 

Not really sure best way to proceed to disable the capacitive control and add the resistive?

 

Any insight would be appreciated.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
October 15, 2025

Hello,

Not sure how you will do that mechanically. Is it another LCD having TSC2046IPWR controller integrated or you need to use the same LCD on the board and replace the touch screen film and replace it with another.. 

From electrical and programming stand point, the controller is using a serial interface mostly a SPI interface:

mALLEm_1-1760519269707.png

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
October 15, 2025

Hello,

Not sure how you will do that mechanically. Is it another LCD having TSC2046IPWR controller integrated or you need to use the same LCD on the board and replace the touch screen film and replace it with another.. 

From electrical and programming stand point, the controller is using a serial interface mostly a SPI interface:

mALLEm_1-1760519269707.png

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.