Skip to main content
Senior III
June 21, 2025
Question

STM32F4xx Maker Board Design

Hello,

I want to try this open-source project. 

https://www.pcbway.com/project/shareproject/STM32F4xx_Maker_PCB_MakerST_1_ab9866e3.html

It's based on an STM32F4xx microcontroller and appears to be designed for general-purpose prototyping. I had a few questions after reviewing the schematic and layout, and I was hoping someone with experience in custom STM32 board design could shed some light:

  1. Boot Mode Configuration:
    How does this board handle BOOT0 selection? I couldn't clearly identify if there's a jumper, switch, or default pull configuration. Is it safe to assume it's hardwired to always boot from flash?

  2. SWD Debugging Interface:
    The board exposes the SWD pins, but I didn’t find much detail on signal integrity (length matching, protection resistors, etc.). Are there any known limitations or considerations when using a low-cost ST-Link or J-Link with this kind of layout?

  3. Power Supply Design:
    The project uses a USB Type-C connector for power, but I’m unsure if it follows proper USB PD or if it's limited to 5V basic mode. Has anyone used this exact design and faced any issues powering the board or during USB programming?Thanks in advance. 

This topic has been closed for replies.

1 reply

Mike_ST
ST Technical Moderator
June 27, 2025

Hello,

1) SW3 is for boot mode selection. Please check the schematic available on github.

2) Using a genuine ST-Link probe can help, cheap ones can be unsupported clones. For signal integrity, I'm not sure this is something you have to be worry for the SWD interface, maybe ask the developper on github.

3) STM32F4 has no USB-PD HW block, this design has 5.1k pull-down resistors on CC1/CC2 lines for simple sink mode operation.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.