Skip to main content
Associate
Sep 8, 2025 3:01 PM UTC
Solved

STM32F479 DSI configuration for CO5300

Hello everyone,

I want to use a C05300 based display with DSI. 

I can write and read in LP mode, but not in HS mode. I guess it's a timing problem.

As seen from datasheet, 

CDecouen_0-1757338207561.png

UI should be more than 2ns, so I use a 500MHz bit clock.

CDecouen_1-1757340572018.png

I use 24 bit data format to send data over DSI, so Pixel Clk = 480 x 2 / 24 = 40 MHz. 

I there something I miss?

This topic has been closed for replies.
CDecouenBest answer
Associate
Sep 8, 2025 11:31 PM UTC

Hi there, it seems that despite the datasheet specify there are two data lanes, only one is used... Unless there is something else to setup.

8 replies

CDecouenAuthorBest answer
Associate
Sep 8, 2025 11:31 PM UTC

Hi there, it seems that despite the datasheet specify there are two data lanes, only one is used... Unless there is something else to setup.

ST Technical Moderator
Sep 9, 2025 6:09 AM UTC

Hello @CDecouen 

I recommend you have a look at this AN4860 Application note related to DSI Host on STM32 MCUs, providing guidelines and practical examples on how to configure the DSI Host depending on the operating mode.

Check the DSI PHY timings and DSI config on HS mode are compliant with the specification provided in the AN4860.

Can you try the DSI example in STM32CubeF4 firmware and update it according to your need. For example on : STM32CubeF4/Projects/STM32469I_EVAL/Examples/LCD_DSI at master · STMicroelectronics/STM32CubeF4 · GitHub

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
CDecouenAuthor
Associate
Sep 9, 2025 2:30 PM UTC

Yes, AN4860 and AN4861 are must see before beginning display projects.

Associate
Sep 29, 2025 10:04 AM UTC

Hi @CDecouen , I am also looking to use CO5300 display for my project.
Can you please provide information about
LCD_VFP, LCD_HFP, LCD_VSA, LCD_VBP, LCD_HSA, LCD_HBP ?

 

CDecouenAuthor
Associate
Sep 29, 2025 12:36 PM UTC

Hi @HareshPrajapati, here is the configuration I use for LTDC

CDecouen_0-1759149283272.png

 

 

Associate
Sep 29, 2025 1:11 PM UTC

Thanks @CDecouen 

here is my init code for the display with 180 degree rotation. its seems to working but not as accpected
do you think my 

Set column/row (example payloads) is okay?




 HAL_Delay(100);
 // Page 0
 HAL_DSI_ShortWrite(&hdsi, 0, DSI_DCS_SHORT_PKT_WRITE_P1, 0xFE, 0x00);

 // TE ON
 HAL_DSI_ShortWrite(&hdsi, 0, DSI_DCS_SHORT_PKT_WRITE_P1, 0x35, 0x00);

 // Ctrl Display
 HAL_DSI_ShortWrite(&hdsi, 0, DSI_DCS_SHORT_PKT_WRITE_P1, 0x53, 0x20);

 // Brightness
 HAL_DSI_ShortWrite(&hdsi, 0, DSI_DCS_SHORT_PKT_WRITE_P1, 0x51, 0x80); // 50% brightness
 HAL_DSI_ShortWrite(&hdsi, 0, DSI_DCS_SHORT_PKT_WRITE_P1, 0x63, 0x00);

 uint8_t madctl = 0xC0; // MX=1 → horizontal mirror
// uint8_t madctl = 0x80; // MY=1 → vertical mirror
// uint8_t madctl = 0x60; // MX=1 + MY=1 → 180° flip
 HAL_DSI_LongWrite(&hdsi, 0, DSI_DCS_LONG_PKT_WRITE, 2, 0x36, &madctl);
// CO5300_SetRotation(2);

 // Set column/row (example payloads)
 uint8_t col[] = {0x00,0x08,0x01,0xD9};
 uint8_t row[] = {0x00,0x00,0x01,0xD1};
 HAL_DSI_LongWrite(&hdsi, 0, DSI_GEN_LONG_PKT_WRITE, 5, 0x2A, col);
 HAL_DSI_LongWrite(&hdsi, 0, DSI_GEN_LONG_PKT_WRITE, 5, 0x2B, row);


 // Sleep Out, Display ON
 HAL_Delay(100);
 HAL_DSI_ShortWrite(&hdsi, 0, DSI_DCS_SHORT_PKT_WRITE_P0, 0x11, 0);
 HAL_Delay(100);
 HAL_DSI_ShortWrite(&hdsi, 0, DSI_DCS_SHORT_PKT_WRITE_P0, 0x29, 0);
 HAL_Delay(120);

 

CDecouenAuthor
Associate
Sep 29, 2025 1:24 PM UTC

I have 0xFF  for register #0x63

column and row start depends on display manufacturer. I use 00,06,01,D7 for columns and same as you for rows.

Hope this help, tuning those display parameters is very tricky

 

 

Associate
Oct 1, 2025 3:56 AM UTC

Thanks again @CDecouen .
If you share your .ioc file for DSI configuration then it will be really appriociated.
I am still facing some rendereing issues with display