Skip to main content
Associate
Nov 11, 2025 9:34 PM UTC
Question

STM32F411 and SD card read/write issues (SDIO)

Hi,
I am running a code to expect to get a digital ouput (wave file from sd card) using amplifiermax98357a. when i run this code the only thing i got is a noise like burning wood. can i get any help. i am assuming the sd card not beeing read or initiate to get the file play.

/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __MAIN_H
#define __MAIN_H

#ifdef __cplusplus
extern "C" {
#endif

/* Includes ------------------------------------------------------------------*/
#include "stm32f4xx_hal.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Exported types ------------------------------------------------------------*/
/* USER CODE BEGIN ET */

/* USER CODE END ET */

/* Exported constants --------------------------------------------------------*/
/* USER CODE BEGIN EC */

/* USER CODE END EC */

/* Exported macro ------------------------------------------------------------*/
/* USER CODE BEGIN EM */

/* USER CODE END EM */

/* Exported functions prototypes ---------------------------------------------*/
void Error_Handler(void);

/* USER CODE BEGIN EFP */

/* USER CODE END EFP */

/* Private defines -----------------------------------------------------------*/
#define LED_Pin GPIO_PIN_13
#define LED_GPIO_Port GPIOC
#define BTN_Pin GPIO_PIN_0
#define BTN_GPIO_Port GPIOC
#define BTN_EXTI_IRQn EXTI0_IRQn
#define SD_DET_Pin GPIO_PIN_15
#define SD_DET_GPIO_Port GPIOA

/* USER CODE BEGIN Private defines */

// SDIO Pin Definitions
#define SDIO_CMD_Pin GPIO_PIN_6
#define SDIO_CMD_GPIO_Port GPIOA

#define SDIO_D1_Pin GPIO_PIN_8
#define SDIO_D1_GPIO_Port GPIOA

#define SDIO_D2_Pin GPIO_PIN_9
#define SDIO_D2_GPIO_Port GPIOA

#define SDIO_D0_Pin GPIO_PIN_4
#define SDIO_D0_GPIO_Port GPIOB

#define SDIO_D3_Pin GPIO_PIN_5
#define SDIO_D3_GPIO_Port GPIOB

#define SDIO_CK_Pin GPIO_PIN_15
#define SDIO_CK_GPIO_Port GPIOB

// I2S Pin Definitions for MAX98357
#define I2S_WS_Pin GPIO_PIN_4
#define I2S_WS_GPIO_Port GPIOA

#define I2S_CK_Pin GPIO_PIN_5
#define I2S_CK_GPIO_Port GPIOA

#define I2S_SD_Pin GPIO_PIN_7
#define I2S_SD_GPIO_Port GPIOA

// Add these back - they're needed for BSP_SD_IsDetected()
#define SD_DETECT_PIN SD_DET_Pin
#define SD_DETECT_GPIO_PORT SD_DET_GPIO_Port
#define SD_PRESENT 0
#define SD_NOT_PRESENT 1

/* USER CODE END Private defines */

#ifdef __cplusplus
}
#endif

#endif /* __MAIN_H */

3 replies

Tesla DeLorean
Guru
Nov 11, 2025 11:30 PM UTC

Take the SD Card out of the equation. Make a sine wave in memory and play that.

A .WAV file has headers and can come in many different data formats, ie mono, stereo, 8-bit or 16-bit, etc.

Check you are managing signing, endian, etc properly.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mt19Author
Associate
Nov 12, 2025 2:19 AM UTC

Hi Tesla, thanks for the feedback. I already test the set up with sine wave, it works fine.

Now i am jumping to add sd card where i have a some files to run through amplifier instead of wave fine. I am new on stm32 and field of programming. I am sure because the sd card is not initiated when running the code which mean no f_mount i had the noise instead. But I don't know where exactly the error leading to this outcome.

mt19Author
Associate
Nov 12, 2025 2:30 AM UTC

I am using blackpill STM32F411CEU6, max98357a, pzsmocn sd socket and speaker. The wave file i have is mono, 16bits, 48MHz