Skip to main content
alertjean
Associate
December 11, 2012
Question

STM32F3Discovery : Unknown target connected / Keil

Posted on December 11, 2012 at 20:56

I just got a new STM32F3Discovery board and when I am trying to start a debug session using Keil, it is giving me an error saying ''unknown target connected'' and it fails to download code into the flash. Has anyone faced this issue before ? Are there any solutions ?

I am able to read & erase flash using STlink utility/V2. I am able to download code using the same, but seems like device is not running the downloaded code. All I see the PWR and COM LEDs lit up red.

I also have STM32F4Discovery board which works without any issues.

I use the following versions:

IDE-Version: �Vision V4.60.0.0

Tool Version Numbers:

Toolchain:        MDK-Lite  Version: 4.60.0.0

Toolchain Path:    C:\Keil\ARM\ARMCC\bin\

C Compiler:         Armcc.Exe

Assembler:          Armasm.Exe       V5.02.0.28

Linker/Locator:     ArmLink.Exe       V5.02.0.28

Librarian:             ArmAr.Exe       V5.02.0.28

Hex Converter:      FromElf.Exe       V5.02.0.28

CPU DLL:               SARMCM3.DLL       V4.60.0.0

Dialog DLL:         DARMSTM.DLL       V1.64.0.0

Target DLL:         STLink\ST-LINKIII-KEIL.dll

Dialog DLL:         TARMSTM.DLL       V1.64.0.0

STM32F3Discovery Firmware Version: V2.J16.S0 JTAG Debugger (As shown by ST-Link Utility)

Library Version : STM32F3-Discovery_FW_V1.1.0

#stm32f3discovery-keil
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
December 11, 2012
Posted on December 11, 2012 at 22:02

Has anyone faced this issue before ? Are there any solutions ?

Indeed it's been discussed here before.

Check your Debug/Utilities tabs under the project options.

Make sure to use ''ST-Link Debugger'' and NOT ''ST-Link (Deprecated Version)''
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
alertjean
alertjeanAuthor
Associate
December 11, 2012
Posted on December 11, 2012 at 22:25

Thanks for clarifying that it is indeed the solutionf. I had tried that option earlier but it resulted in an error:

No Algorithm found for: 08000000H - 0800412BH

On further probing I found that in ST-Link Debugger > Settings > Flash Download  I had to pick STM32f3xx Flash 256k( Or should I pick size 16). It programs correctly once that is done.

Thanks anyway!.

John Griswold
Senior
February 14, 2018
Posted on February 14, 2018 at 18:50

And in 2018, this still works! Thanks

eng239955
Associate
March 1, 2013
Posted on March 01, 2013 at 10:58

No Algorithm found for: 08000000h -080038a3h

i faced this  problem  with stm32f4 discovery 

in keil-mdk

i found that i have to add stm32f4 flash  in {programming algorithm }

project->option for target -> utilities ->settings ->add ->stm32f4xx flash 
610312521
Visitor II
June 10, 2013
Posted on June 10, 2013 at 03:34

change the settings in here {options-utilities-settings-debug-ort(change gtag to sw)}