Skip to main content
Associate III
July 11, 2025
Solved

STM32F303CCT6 - SPI1 Prescaler Issue (Can't Set to 2)

  • July 11, 2025
  • 1 reply
  • 1298 views

Hi everyone,

I'm working with the STM32F303CCT6 chip, and I've configured the system clock such that HCLK is running at 72 MHz.

I'm trying to configure SPI1 in full-duplex master mode using CubeMX / STM32CubeIDE. However, when I attempt to set the prescaler to 2, it gives me the following warning:

"With this Prescaler value and APB2 Clock Frequency (72.0 MHz), Baud Rate is more than 18.0 MBits/s.
Please set Prescaler more than 4."

This is confusing because I thought SPI1 could go up to 32 Mbit/s.

Has anyone encountered this?

  • Is this a limitation from CubeMX or HAL?

  • Is it safe to ignore this warning and proceed manually in code?

  • Or is there a hardware limitation I'm overlooking?

Any insights or workarounds would be greatly appreciated!

Thanks in advance!Screenshot 2025-07-11 174915.png

This topic has been closed for replies.
Best answer by KDJEM.1

Hello @Shreayas_Acharaya;

 

As mentioned in the datasheet DS9118 Rev 14 Section 3.22 Serial peripheral interface (SPI)/Inter-integrated sound interfaces (I2S) the SPIs are able to communicate up to 18Mbits/s: "three SPIs are able to communicate up to 18 Mbits/s in slave and master modes in full-duplex and half-duplex communication modes" 

KDJEM1_0-1752485576021.png

 

Thank you.

Kaouthar

 

1 reply

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
July 14, 2025

Hello @Shreayas_Acharaya;

 

As mentioned in the datasheet DS9118 Rev 14 Section 3.22 Serial peripheral interface (SPI)/Inter-integrated sound interfaces (I2S) the SPIs are able to communicate up to 18Mbits/s: "three SPIs are able to communicate up to 18 Mbits/s in slave and master modes in full-duplex and half-duplex communication modes" 

KDJEM1_0-1752485576021.png

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.