Skip to main content
woermann
Visitor II
February 26, 2016
Question

STM32f0 - I2C EEprom > 1Mbit - i cant get it run.

Posted on February 26, 2016 at 13:57

Dear Madams and Sirs,

im trying to programming / and reading an 1Mbit EEprom with STM32F030x.

There are some issues i am working on and make me some headache.

Im using the STM32f0xx_i2c files for working and a Keil Compiler

(V5.17).

My first problem is:

Im using one of our internal libarys to write and read to the eeprom. It

is programmed as discriebed in the the STM Reference Manual and worked

fine with EEprom values lower 1Mbit.

I added a second adress byte to the adressing and put the value of

sending bits in the I2C_TransferHandling to 2.

But when im looking to the data with a Osciloscop I see only one adress

byte. In case of writing it seems that the 2nd one is puting to data

(because i have to rise the data by one to the former version). In case

of reading the start byte / device select byte for reading  will be send

after the 1st Adressbyte. The 2nd adress byte is missing.

The other issue is: When im putting the 2nd Adress byte to the code the

routine will not more handle the waiting for the TXIS flag after setting

I2C_TransferHandling at the start. It looks like hanging up there. This

work also fine, when i'm only using one byte of adressing.

I try to programm the routine new, in a different way - by using

I2C_SlaveAddressConfig(); I2C_NumberOfBytesConfig(); I2C_SendData() and

try it a the write routine. This didn't work either with the same

result. the starting routing stopps after the first adress byte.

Does somebody has an example for this task or an idea what is going

wrong?

Kind regards

Jens

#i2c #eeprom #1mbit
This topic has been closed for replies.