Kg_itAssociate7 years agoJun 25, 2019 8:25 AM UTCQuestionSTM32-MAT TARGET work with matlab2019a error:" Reference to non-existent field 'codeFormat'."1 reply1495 viewsI use the STM32demo /PIL/"Filter" with the matlab 2019a, Then , I get the next information And when I used the matlab 2018b, there are some others errors"invalid index"", if the STM32-MAT target is older ? so which matlab version is best matching? @Amel NASRI @PascalRTest_PIL_IIR_Filter2018_simulation_20190625_160559.txtSTM32-MatTarget