Skip to main content
julio
Associate II
July 5, 2016
Question

STM32 Mat/Target problem PIL mode

Posted on July 05, 2016 at 13:07

Hi everyone!

I have developed a very simple code to test the STM32 Mat/Target. It works properly in normal mode, but when I try to use the ''Processor in the Loop'' mode (PIL) to view in simulink the state of an input, the KVM v5 shows this error:

compiling rt_main.c...

..\aaa\Src\rt_main.c(32): error:  &sharp35: &sharperror directive: Must specify a model name.  Define MODEL=name.

  ♯ error Must specify a model name.  Define MODEL=name.

How can I fix it? Any help?

Thanks!

#stm32-mat-target
This topic has been closed for replies.

4 replies

slimen
Visitor II
July 5, 2016
Posted on July 05, 2016 at 14:46

Hi p92lomij,

It should be a ''bad'' configuration as you should not have rt_main.c file!

You can refer to the attached manual (STM32-MAT/TARGET

Hands On) it will help you in your configuration.

Regards

________________

Attachments :

STM32_MAT-TARGET_HandsOn_v1_0.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htol&d=%2Fa%2F0X0000000aXC%2FrCcaoZUmkCfBHqg8nkz23x_gA_.BNoVO2e3pNoF.fxw&asPdf=false
florence
Associate II
July 9, 2016
Posted on July 09, 2016 at 03:08

Could you tell me where and how I can launch the matlab app GUI show on page 34 of this hand on manual, so that I can configure the COM port for the PIL test?

Stefano Albertini
Visitor II
April 12, 2018
Posted on April 12, 2018 at 21:47

Hello,

I have the same problem.

My system is set correctly but when I try to compile Keil progect the same error was shown:

compiling rt_main.c...

..\Src\rt_main.c(32): error:  #35: #error directive: Must specify a model name.  Define MODEL=name.

  # error Must specify a model name.  Define MODEL=name.

I follow the readme.pdf step by step and I don't think it's a wrong set of matlab or simulink.

I've also read the main_rt shouldn't be generated, maybe some problems with keil or with cubeMX?

IDE-Version:

µVision V5.24.2.0

Tool Version Numbers:

Toolchain:        MDK-ARM Plus  Version: 5.24.1

Toolchain Path:    C:\Keil\ARM\ARMCC\Bin

C Compiler:         Armcc.exe        V5.06 update 5 (build 528)

Assembler:          Armasm.exe        V5.06 update 5 (build 528)

Linker/Locator:     ArmLink.exe        V5.06 update 5 (build 528)

Library Manager:    ArmAr.exe        V5.06 update 5 (build 528)

Hex Converter:      FromElf.exe        V5.06 update 5 (build 528)

CPU DLL:               SARMCM3.DLL          V5.24.1

Dialog DLL:         DCM.DLL              V1.16.0.0

Target DLL:             STLink\ST-LINKIII-KEIL_SWO.dll      V3.0.1.0

Dialog DLL:         TCM.DLL              V1.32.0.00690X0000060AZPQA2.png

Could you help me please?

Visitor II
April 17, 2018
Posted on April 17, 2018 at 04:01

Hello,

stefano.albertini

Could you please give me more information?

Which STM32 board you use?

If you provide a little test case if possible or at least an simulink file.

Thanks.