Skip to main content
a m
Associate II
Feb 19, 2018 6:32 AM UTC
Question

STM32 MAT/TARGET 4.4.2 ADC has bug

Posted on February 19, 2018 at 07:32

hello

when I use code generation,  I see the ADC block is disconnected!

matlab 2016b

stm32 MAT/TARGET 4.4.2

This topic has been closed for replies.

7 replies

Visitor II
Feb 19, 2018 9:43 AM UTC
Posted on February 19, 2018 at 10:43

Hello, Sir

Could you please give me more information?

for example:

- which STM32 you use?

- If you provide a little test case if possible or at least an ioc file and Simulink file.

Thanks,

a m
a mAuthor
Associate II
Feb 21, 2018 6:42 AM UTC
Posted on February 21, 2018 at 06:42

I reinstalled the software and STM32 respond when I tried to provide a little test case!

I think it was my mistake, sorry for wasting your time.

thank you for your respond.

Visitor II
Feb 21, 2018 7:09 AM UTC
Posted on February 21, 2018 at 07:09

Is it works now? I

f you found cause of problem 

please

describe 

how you resolved 

because it will helpful for 

of future readers with the same problem.

Best regards,

nailgg
Visitor II
Sep 9, 2018 3:34 PM UTC

Hello,

I also have the same problem. When I generate the code for my target, ADC block becomes disconnected! It looks like the output pins of the ADC read block are refreshed when I generate the code, and as a result, it's disconnected. It doesn't happen on the ADC interrupt block but only happens on channel reading block.

Matlab version is R2018a, and my target device is STM32F103RB. I tried reinstalling the STM32-MAT but it didn't help. Any advice?