Skip to main content
Attila Szabo
Associate
Jan 13, 2023 7:57 AM UTC
Question

STM32 internal eeprom

Hi!

I am working with a STM32L053 MCU. I would like to write to the internal eeprom, and based on the datasheet it takes 3.2 ms.

I have doubts that during that time interrupts will be ignored. It is not clear for me why. 

I thought that the code is in the flash and the eeprom is independent from the flash. 

(Or maybe this EEPROM is not a real EEPROM, but emulated EEPROM in flash?)

Best regards

This topic has been closed for replies.

1 reply

RomainR.
ST Employee
Jan 13, 2023 1:57 PM UTC
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.