Skip to main content
Senior
Feb 17, 2026 12:04 PM UTC
Solved

STM32 Driver for GOODIX GT911 touch controller

Hey, I am using the RK043FN66HS-CTG LCD touchscreen (480 x 272 resolution) and have used the GT911 drivers found at:

GitHub - DiveInEmbedded/GT911-Touch-driver: Simple and ready to use touch driver for Goodix GT911

I have a custom STM32H743IIT6 PCB.It is currently recording coordinates incorrectly in the y- axis. Bottom right hand corner should be 480,272 (X,Y) roughly in landscape configuration. I am getting ~440,180.

I have gone through the GT911 Register Datasheet but cannot seem to figure out why the readings are still off.

Any suggestions why I am getting these issues. I understand the config version register has to be increment by one with each set of GT911 settings.

 

My GT911 Config is here:

 
static uint8_t GT911_Config[] =

{

0x89, // Config version

0xE0, 0x01, // X = 480

0x10, 0x01, // Y = 272

0x05, // 5 touch points

0x40, // ModuleSwitch1 (landscape, no flip)

0x20, 0x01, 0x08, 0x28, 0x05, 0x50,

0x3C, 0x0F, 0x05, 0x00, 0x00, 0x00, 0x00, 0x00,

0x00, 0x00, 0x00, 0x00, 0x00, 0x00,

0x00, 0x89, 0x2A, 0x0B, 0x2D, 0x2B, 0x0F, 0x0A,

0x00, 0x00, 0x01, 0xA9, 0x03, 0x2D, 0x00, 0x01,

0x00, 0x00, 0x00, 0x03, 0x00, 0x00, 0x00, 0x00,

0x00, 0x21, 0x59, 0x94, 0xC5, 0x02, 0x07, 0x00,

0x00, 0x04, 0x93, 0x24, 0x00, 0x7D, 0x2C, 0x00,

0x6B, 0x36, 0x00, 0x5D, 0x42, 0x00, 0x53, 0x50,

0x00, 0x53,

// Padding zeros

0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,

0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,

0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,

// Sensor tuning

0x02,0x04,0x06,0x08,0x0A,0x0C,0x0E,0x10,

0x12,0x14,0x16,0xFF,0xFF,0xFF,

// More padding

0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,

// Final tuning

0x02,0x04,0x06,0x08,0x0A,0x0F,0x10,0x12,

0x16,0x18,0x1C,0x1D,0x1E,0x1F,0x20,0x21,

0x22,0x24,

// Padding

0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,

0x00,0x00,0x00,0x00,0x00,0x00,0x00,

// Checksum (filled by code)

0x00,

// Config fresh flag

0x01

};

 

 

AEng7Best answer
Senior
Feb 19, 2026 9:10 AM UTC

This issue was solved.

 

I used a second RK043FN66HS-CTG and the waveshare code provided by https://github.com/DiveInEmbedded/GT911-Touch-driver/tree/main on the drivers page.

 

AEng7_0-1771492145657.png

 

I would assume using the original driver wrote to registers it should not have modified. 

Using a new RK043FN66HS-CTG means the touchscreen just works with expected coordinates using the waveshare drivers. 

 

Only modification to the waveshare driver was to modify the width and height to 480 and 272. The origin (0,0)  matched that of TouchGFX.

 

2 replies

AEng7Author
Senior
Feb 18, 2026 6:09 PM UTC

Anyone?

 

I noticed when not reversing x and y, and not swapping axis. I reach roughly 480,270 in the left corner so the origin 0,0 is in the bottom right corner.

but it is not compatible with TouchGFX and its origin placement.

 

obviously when I reverse the axis in hardware or software it seems off and clips the x axis.

 

also noticed the centre point is off, hence me asking for registers of this device.

AEng7AuthorBest answer
Senior
Feb 19, 2026 9:10 AM UTC

This issue was solved.

 

I used a second RK043FN66HS-CTG and the waveshare code provided by https://github.com/DiveInEmbedded/GT911-Touch-driver/tree/main on the drivers page.

 

AEng7_0-1771492145657.png

 

I would assume using the original driver wrote to registers it should not have modified. 

Using a new RK043FN66HS-CTG means the touchscreen just works with expected coordinates using the waveshare drivers. 

 

Only modification to the waveshare driver was to modify the width and height to 480 and 272. The origin (0,0)  matched that of TouchGFX.