Skip to main content
YBAYR.1
Associate III
May 21, 2024
Question

stm32 code to control brightness of 2 lamps using 2 triacs

  • May 21, 2024
  • 4 replies
  • 3522 views

Merhaba 2 triyak kesinti ile araç kullanmak istiyorum bunun için ne yapmalıyım? 50hz 220v şebeke elektriğini kullanıyorum. 0 noktasını tespit ettikten sonra belli bir süre bekleyip ardından triyak'a darbe veriyorum. İkinci darbe değerini verdiğimde sistem karışıyor.

 

kodum ek dosyada:

YBAYR1_0-1716300238623.png

 

This topic has been closed for replies.

4 replies

mƎALLEm
ST Technical Moderator
May 21, 2024

Hello,

Please write in English as it's an international community so you will have more chance to get support from the members.

Thank you for your understanding.

Translation:

Hello, I want to drive with 2 triac interruptions, what should I do for this? I use 50hz 220v mains electricity. After detecting point 0, I wait for a certain period of time and then pulse the triac. When I give the second pulse value, the system gets confused.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Muhammed Güler
Senior III
May 21, 2024

öncelikle google translate ile de olsa sorununu ingilizce yazman gerekiyor.

Coming to your question, using delay in interrupt is a big mistake.
Within exti interrupt; You should do short tasks like checking outputs, setting and starting timers.
Or you can change the value of a variable in the interrupt and check it in the main loop.
There are many approaches, the important thing is to get out of the interrupt as quickly as possible

YBAYR.1
YBAYR.1Author
Associate III
May 21, 2024

Muhammed bey size linkedin üzerinden ulaşabilir miyim?

I'm having problems with the language, thank you for your reply