Skip to main content
RGate.15
Associate
Mar 21, 2019 6:49 PM UTC
Question

Start the project with STM32F769I-EVAL board using Atollic TrueStudio and STM32CubeMX 5.1.0

I have a STM32F769I-EVAL board and am using Atollc TrueStudio development tools and STM32CubeMX 5.1.0 to start the project.

This topic has been closed for replies.

2 replies

ST Technical Moderator
Mar 22, 2019 8:51 AM UTC

Hello,

Do you face any problem to start your project?

The STM32CubeF7 firmware package provides a rich set of examples and applications that helps you:

STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I_EVAL

Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
RGate.15
RGate.15Author
Associate
Mar 22, 2019 2:25 PM UTC

​I was trying to copy information into my original post when it sent the post before I was ready.  I have a project and it compiles with the Atollic tool set.  When I go to debug it, I get the following message:

Failed to execute MI command:

-file-exec-and-symbols C:/Users/rgate/Desktop/Third/Third.elf.launch

Error message from debugger back end:

"C:/Users/rgate/Desktop/Third/Third.elf.launch": not in executable format: File format not recognized

The board had been used for a previous project and so the demo software is not installed in it.