Skip to main content
darla14
Associate III
January 6, 2016
Question

Sending Stream of Inputs froma file to IAR code using Terminal I/O

Posted on January 06, 2016 at 05:35

Hi Everyone, 

Is there a way of using Terminal I/O feature of IAR(or any other)to send large input values(string or binary)) to function getting executed on STM32 Nucleo board.The input values being read from the text file placed on the Development PC.

This is required to test some image processing functions in IAR which requires lot of Test data to be processed inside the code running on IAR.

Thanks in advance !

Rgds,

Rp

#nucleo #iar #keil #!stm32 #stm32cubemx
This topic has been closed for replies.