Skip to main content
Visitor II
Apr 16, 2025 1:20 PM UTC
Question

RF LTE-M evaluation on B-L462E-CELL1

Hello,

I'm working on LTE-M protocol and I would like to use B-L462E-CELL1 to evaluate the RF performances and characteristics of LTE-M protocol.
I would like to know, if it test tools/software to control the LTE-M chip in order to be the wanted mode is released or not?
I need this test software to program the RF device to transmit or receive mode, by defining the frenquecy and the transmit power... In order to test the following items:
- Tx Power / Frequency error
- Modulation accuracy
- Spectrum Mask
- Channel Testing
- Sensitivity

Could you please specify if this kind of control is possible and could be delivered for B-L462E-CELL1?
Thanks and Best Regards,
Asmaa

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
Apr 16, 2025 2:13 PM UTC

Welcome @Asmaa, to the community!

The LTE-M module in the B-L462E-CELL1 is from Murata, who you should contact for such special requests. However, such modules have also been discussed here in the community, e.g. here.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.