Skip to main content
NCTUser
Associate II
Feb 4, 2019 7:14 AM UTC
Question

Remote failure reply: E31

Hello,

I use TrueSTUDIO 9.2.0 and I sometimes get the following

error:

warning: Remote failure reply: E31

C:\Users\***\AppData\Local\Temp\truestudio8442355296883488729gdbscript:14: Error in sourced command file:

Remote communication error. Target disconnected.: No error.

This is a bug, please report it. For instructions, see:

http://www.gnu.org/software/gdb/bugs/.

/home/build/gcc-arm-none-eabi-6-2017-q1-update/src/gdb/gdb/thread.c:817: internal-error: is_thread_state: Assertion `tp' failed.

A problem internal to GDB has been detected,

further debugging may prove unreliable.

Quit this debugging session? (y or n) [answered Y; input not from terminal]

/home/build/gcc-arm-none-eabi-6-2017-q1-update/src/gdb/gdb/thread.c:817: internal-error: is_thread_state: Assertion `tp' failed.

A problem internal to GDB has been detected,

further debugging may prove unreliable.

Create a core file of GDB? (y or n) [answered Y; input not from terminal]

I can't debug my project and I should recover my project

from backup. I do not want to report the error because I

dont know how to reproduce it. Can anyone faced similar

error? How can I "reset" the TS/GDB settings without

recovering the whole workspace from backup?

This topic has been closed for replies.