Skip to main content
MNoor.10
Visitor II
Jan 15, 2019 3:47 AM UTC
Question

__RBIT() and Truestudio

I want to reverse the Bits of a unsigned long data that is acquired by serial port. I used __RBIT() function in Attolic Truestudio but it does not work . I found during debugging the ARM_ARCH_7M  is not defined .

I compiled similar code in the KEIL , it works well. Kindly guide me in this regard.

This topic has been closed for replies.

3 replies

AvaTar
Senior III
Jan 15, 2019 11:11 AM UTC

Why not using the C language operators (~, one's complement), instead of macros with questionable portability ?

waclawek.jan
Super User
Jan 15, 2019 11:53 AM UTC

AvaTar,

this is about bit reversal, i.e. "mirroring" the word, changing the bit ordering; not bit inversion/negating.

jehanzebnoorpuri,

I don't use Atollic, but in your source you should have included stm32f7xx.h, that should include the header for your particular STM32 model, that should include core_cm7.h, that should include core_cmFunc.h , and that for gcc should include cmsis_gcc.h, and that should include definition of __RBIT() as a static inline function. Go along that chain.

JW

AvaTar
Senior III
Jan 15, 2019 12:58 PM UTC

You're right - my bad.

Bit shuffling, as it's called in the e.g. in the FFT context.