Associate
Oct 16, 2018 4:05 PM UTC
Question
PWM Linker Issue on IAR with Simulink generated code
- 7 replies
- 5297 views
I'm having an issue with the timer block in the STM32 blockset in simulink setting it up for the STM32F030F4P6 processor. The project builds fine in simulink but when I build in IAR I get a linker error, see attached image. I've attached images showing the settings used in STM32CUBEMX and the errors in IAR. I'm using the most up to date version of the firmware on the ST website v1.9. I'm hoping this is just a setup issue that I can't seem to figure out. Any help is appreciated.