Skip to main content
VBazh
Visitor II
Jun 27, 2019 11:35 AM UTC
Question

Problems with the project STM32L476G-Discovery Demonstration

I try to create a project from directory (STM32Cube_FW_L4_V1.14.0\Projects\32L476GDISCOVERY\Demonstrations\TrueSTUDIO). It creates two projects: "TrueSTUDIO" and "STM32L476G-Discovery" . The file TrueSTUDIO_converter.log is generated in the folder TrueSTUDIO. It says:

Project: TrueSTUDIO

Converter: IARProjectParser

Date: 20190627

Failed to parse IAR project format file, if possible please send the Project.ewp file together with the workspace log file to Atollic support.

When I try to build the project "STM32L476G-Discovery" an error occures:

...

In file included from ..\..\..\Core\Src\main.c:34:0:

../../../Modules/guitartuner/guitartuner.h:33:22: fatal error: arm_math.h: No such file or directory

 #include "arm_math.h"

           ^

compilation terminated.

21:24:44 Build Finished (took 39s.82ms)

Could anybody help me?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Jun 27, 2019 11:39 AM UTC

Make sure you have Include paths defined in the project so it knows where to search for CMSIS include files, or if it copied them to the local project workspace.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..