Skip to main content
pncardella
Associate II
July 21, 2014
Question

Problems During Debugger Mode

Posted on July 21, 2014 at 10:08

I am working with an STM32 eval2 board and trying to debug it. It used to work fine, and I haven´t changed anything, but for the last week or so I am always getting stuck in this loop while I am in debugger mode, but when I am not, the program runs fine.

while(!__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_FLAG_RXOVERR | SDIO_FLAG_DCRCFAIL | SDIO_FLAG_DTIMEOUT | SDIO_FLAG_DBCKEND | SDIO_FLAG_STBITERR)) { if(__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_FLAG_RXDAVL)) { *(tempscr + index) = SDIO_ReadFIFO(hsd->Instance); index++; } }

I even tried running the sample project code provided for the board by ST, did not change anything about it, and I am stuck in the same while loop in their code as well.

Does anybody know what I am doing wrong here? It doesn´t make sense because nothing changed.

The errors that are defined by the variables in the while loop are (respectively):

Received FIFO overrun error

Data block sent/received (CRC check failed) Data timeout Data block sent/received (CRC check passed) Start bit not detected on all data signals in wide bus mode

and it looks like in this while loop it is getting stuck in the if statement for a ''Data available in receive FIFO'' flag, if that makes sense. I cannot step over that if statement.

I am using keil v5 and programming in c++

#eval #keil #stm32f4 #c++
This topic has been closed for replies.

1 reply

pncardella
Associate II
July 21, 2014
Posted on July 21, 2014 at 10:11

Like I said I have had this problem for a week and immediately after I posted this I figured it out. I had the SD card in, and for some reason that was giving me those errors. I will leave this post in case anyone else ever has this problem.