Skip to main content
AWack
Associate III
Mar 18, 2026 5:06 PM UTC
Solved

Porting ST67W6 from Nucleo U575ZI to custom baord with U575CI fails

Hi,

I´m trying to migrate the example Application p2pServer (BLE) from the Nucleo board to a custom board with an STM32U575CI, but it fails initializing:

#### Welcome to ST67W6X BLE P2P Server Application #####<\n>
# build: 17:52:14 Mar 18 2026<\n>
--------------- Host info ---------------<\n>
Host FW Version: 1.2.0<\n>
[ERROR] [4000] [ST67W6XTask] (w61_at_sys.c:340) sem_if_ready not received<\n>
[ERROR] [4000] [ST67W6XTask] (w61_at_common.c:375) sem_if_ready not received<\n>
[ERROR] [4000] [ST67W6XTask] (w61_at_sys.c:312) Could not init Modem handler<\n>
[ERROR] [4000] [ST67W6XTask] (main_app.c:975) [ERROR] in W6X_Init API<\n>
[ERROR] [4000] [ST67W6XTask] (w6x_sys.c:115) W61 Init failed<\n>
[ERROR] [4000] [ST67W6XTask] (main_app.c:401) Failed to initialize ST67W6X Driver

Any idea what could be the problem?

Best

Achim

AWack
AWackBest answer
Associate III
Mar 26, 2026 11:22 AM UTC

Now it´s working. I´ve forgotten to set the SPI related IOs to Very High Speed...

3 replies

TDK
Mar 18, 2026 5:22 PM UTC

What is different between the two boards? Start there.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Mar 18, 2026 5:55 PM UTC

@AWack wrote:

I´m trying to migrate the example Application p2pServer (BLE) from the Nucleo board ...


Have you got it working on the Nucleo board?

 


@AWack wrote:

 

... to a custom board with an STM32U575CI


Please show your schematic.

Before the full port, have you proved your basic SPI comms?

Have you used a scope and/or logic analyser to see what's happening on the interfaces between the Host and the ST67W6 ?

Compare & contrast the working & non-working cases ...

Instrument your code so see what's happening.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AWack
AWackAuthorBest answer
Associate III
Mar 26, 2026 11:22 AM UTC

Now it´s working. I´ve forgotten to set the SPI related IOs to Very High Speed...