Skip to main content
Iaomari
Associate II
Feb 21, 2021 1:08 PM UTC
Question

Nucleo-l476RG development kit.

Hi everyone.

I'm new here so please forgive if me questions are basic.

Lately I received Nucleo-l476RG development kit, and for the basic testing I'm using the Arduino IDE to upload the test file.

I'm using Ubuntu 18.04, with Arduino 1.8.13.

compiling the sketch works fine, however, when I try to upload it I got this message

/home/***/snap/arduino/50/.arduino15/packages/STM32/tools/STM32Tools/1.4.0/tools/linux/massStorageCopy.sh: line 71: /bin/df: Permission denied

/home/***/snap/arduino/50/.arduino15/packages/STM32/tools/STM32Tools/1.4.0/tools/linux/massStorageCopy.sh: line 71: /bin/df: Permission denied

NODE_L476RG,NOD_L476RG not found.

Please ensure the device is correctly connected and mounted.

An error occurred while uploading the sketch.

this is the Arduino configuration that I used:

Board : Nucleo-64

Board part number : Nucleo-l476RG

UART support : Enable generic serial

USB support : None

USB speed : LOW/Full speed

optimize : smallest os default

C runtime lib : newLib nano

upload method : mass storage

thank you.

This topic has been closed for replies.

2 replies

ChahinezC
Associate II
Mar 4, 2021 3:03 PM UTC

Hello @Iaomari​,

Welcome to ST community.

Please make sure that you are selecting the right port. I also recommend you checking the USB cable you are using.

Have you tried to use an other Arduino compatible board?

Chahinez.

Iaomari
IaomariAuthor
Associate II
May 26, 2021 8:50 AM UTC

thank you very much