Skip to main content
Associate III
July 31, 2025
Question

Nucleo-H753ZI board Connect ADC inputs to GND, the readings are varied between -15 - +15

Nucleo-H753ZI board. ADC1 configurations: INPUT: SINGLE-END

Sample clock rate = 5Mhz

Sample rate = 10Khz,

Sample Time = 16.5 cycles,

Resolution = 12-bit

Scan 256 times

Connect the defined two ADC input channels to GND.

The 256 readings FOR EACH INPUT are varied between (-15 - +15), more or less, while they should be read as zeros.

Question: Can it be fixed How to fix it?

Could you do the same test to confirm it?

Thanks,

 

Rong

This topic has been closed for replies.

12 replies

Chris21
Associate II
July 31, 2025

The lowest value a single-ended ADC channel can have is 0, how do you get negative numbers?

.
Associate III
July 31, 2025

Sorry, I pasted wrong data. It should be

5, 0, 5, 0, 12, 0, 15, 1, 0, 0, 0, 0, 3, 5, 17, 0, 0, 0, 0, 0, 0, 15, 0, 11, 17, 16, 0, 0, 12, 0, 4, 15, 7, 0, 0, 0, 0, 0, 0, 0, 5, 10,

Total 256's. I just listed first 40's.

Thanks

Associate III
August 1, 2025

5, 0, 5, 0, 12, 0, 15, 1, 0, 0, 0, 0, 3, 5, 17, 0, 0, 0, 0, 0, 0, 15, 0, 11, 17, 16, 0, 0, 12, 0, 4, 15, 7, 0, 0, 0, 0, 0, 0, 0, 5, 10, 14, 0, 0, 0, 4, 13, 0, 13, 0, 0, 0, 0, 1, 0, 0, 0, 0, 16, 8, 0, 16,12, 0, 13, 0, 0, 9, 0, 0, 0, 3, 0, 0, 15, 0, 0, 13, 0, 1, 16, 0, 0, 16, 9, 0, 0, 18, 0, 13, 0, 0, 0, 17, 0, 0, 0, 6, 0...}

Chris21
Associate II
August 1, 2025
Associate III
August 1, 2025

"Are you executing the calibration functions?"

Of course.

Data

5, 0, 5, 0, 12, 0, 15, 1, 0, 0, 0, 0, 3, 5, 17, 0, 0, 0, 0, 0, 0, 15, 0, 11, 17, 16, 0, 0, 12, 0, 4, 15, 7, 0, 0, 0, 0, 0, 0, 0, 5, 10, 14, 0, 0, 0, 4, 13, 0, 13, 0, 0, 0, 0, 1, 0, 0, 0, 0, 16, 8, 0, 16,12, 0, 13, 0, 0, 9, 0, 0, 0, 3, 0, 0, 15, 0, 0, 13, 0, 1, 16, 0, 0, 16, 9, 0, 0, 18, 0, 13, 0, 0, 0, 17, 0, 0, 0, 6, 0...}

Karl Yamashita
Principal
August 1, 2025

@RongShengWang wrote:

"Are you executing the calibration functions?"

Of course.

Data

5, 0, 5, 0, 12, 0, 15, 1, 0, 0, 0, 0, 3, 5, 17, 0, 0, 0, 0, 0, 0, 15, 0, 11, 17, 16, 0, 0, 12, 0, 4, 15, 7, 0, 0, 0, 0, 0, 0, 0, 5, 10, 14, 0, 0, 0, 4, 13, 0, 13, 0, 0, 0, 0, 1, 0, 0, 0, 0, 16, 8, 0, 16,12, 0, 13, 0, 0, 9, 0, 0, 0, 3, 0, 0, 15, 0, 0, 13, 0, 1, 16, 0, 0, 16, 9, 0, 0, 18, 0, 13, 0, 0, 0, 17, 0, 0, 0, 6, 0...}


And to be sure we're all on the same page, how are you exactly calibrating?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source