Skip to main content
Associate
Aug 6, 2025 1:49 PM UTC
Question

Nucleo-F303 + SHT45 - I2C NACK Issue

I needed a very small humidity sensor, so I made a PCB for the Sensirion SHT45. I interface it with a Nucleo-32 F303K8, and have tried a Nucleo 64 as well. It seems that I'm able to send commands to it, but when I try to read it, I receive only NACKs from the sensor. This behaviour could be because of a busy sensor, but I add enough time in between measurement request and reading that it should not be a problem. 

I tried a few chips. The first ones I soldered with an iron, then I tried hot air, most recently hot air from bottom of PCB, to shield the chip and especially its PTFE membrane from the heat of the air. I wonder if solder heat could have broken the sensor in a way where it will respond to I2C, but the sensing element might be broken.

I use CubeIDE, I2C standard default settings.

// Buffer to store RX data
uint8_t buffer[6] = {};

// Request High Precision reading - no error
if(HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)(0x44 << 1),(uint8_t *)0xFD,1, 1) != HAL_OK){
uint8_t dummy = 1;
}

HAL_Delay(200); //have tried delays of 20, 50, 100 and 200 ms

// Reading sensor - always get NACK from sensor, hi2c1 errorcode 4 (NACK error)
HAL_StatusTypeDef ret = HAL_I2C_Master_Receive(&hi2c1, (uint16_t)(0x44 << 1), buffer, 6, 1);
while(ret != HAL_OK) {
ret = HAL_I2C_Master_Receive(&hi2c1, (uint16_t)(0x44 << 1), buffer, 6, 1);
}

HAL_Delay(20);

 

I use 2.2K pull up resistors, and very short soldered wires in my test setup.

averiksen_1-1754488041718.png

Edited to apply source code formatting - please see How to insert source code for future reference.

This topic has been closed for replies.

6 replies

Andrew Neil
Super User
Aug 6, 2025 2:01 PM UTC

@averiksen wrote:

It seems that I'm able to send commands to it


How have you verified that?

 


@averiksen wrote:

but when I try to read it, I receive only NACKs from the sensor.


Have you looked at the I2C lines with an Oscilloscope - are they clean, and with good edges?

Have you decoded what's happening on the lines (eg, with an analyser), and checked it against the SHT45 specifications?

 

Does your I2C work with any other chips?

 


@averiksen wrote:

I wonder if solder heat could have broken the sensor in a way where it will respond to I2C, but the sensing element might be broken.


You'd have to ask Sensirion about that; it's their chip - not ST's.

https://sensirion.com/products/support 

 

Have you tried with a Sensirion evaluation kit?

Or a 3rd-party breakout; eg, https://www.adafruit.com/product/5665 ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
averiksenAuthor
Associate
Aug 6, 2025 2:13 PM UTC

I probed the data lines on a regular scope, the waveforms seem clean. I could see the command being transmitted and acknowledged as one would expect the waveform to look. Additionally, the STM32 HAL returns HAL_OK from the HAL_I2C_Master_Transmit() function.

 

When the HAL_I2C_Master_Receive() executes, I see the sensor address on the data line, but the sensor pulls the data line high (NACK).

START - ADDR + READ-BIT - NACK   ... and nothing more.

 

I used the same Nucleo to read a HYT271 sensor, also humidity, not sensirion though, a while ago. I should try and check that it still works.

I haven't tried with an evaluation kit, but I have a cheap board coming in form Aliexpress soon.

Sensirion details that one should be very careful when handling the sensor, basically using a reflow oven and nothing else, but I was interested in hearing if others have had the experience of soldering one of these chips on a board.

TDK
Aug 6, 2025 2:33 PM UTC

> HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)(0x44 << 1),(uint8_t *)0xFD,1, 1)

This is junk. You want this:

uint8_t data = 0xFD;
HAL_I2C_Master_Transmit(&hi2c1, (uint16_t)(0x44 << 1), &data, 1, 1000);

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
Aug 29, 2025 5:03 PM UTC

You can check if the I2C-communication with a device is ok with HAL_I2C_IsDeviceReady. Also look at the suggestions of @TDK