Skip to main content
Jose Romero
Associate II
Oct 5, 2018 4:15 PM UTC
Question

Motion control in Hexapods !!

Hi, I'm doing a hexapod with 18 servos and 6 legs (3 servos for each leg). I am using a core board and the Mbed environment with C language.

My question is: how could I initially consider the movements?

Initially I have declared all the necessary pins (18) and in which I have passed a pulse to servo number 1 to prove that the pin works on the board. I would like to know how to perform a simple movement even if they are 3 servos that would be 1 leg.

My code is the following:

#include "mbed.h"

#include "SoftPWM.h"

Serial serial(PC_6, PA_12);

SoftPWM servo1(PB_8);

SoftPWM servo2(PB_9);

SoftPWM servo3(PB_7);

SoftPWM servo4(PA_0);

SoftPWM servo5(PA_1);

SoftPWM servo6(PB_0);

SoftPWM servo7(PB_1);

SoftPWM servo8(PA_3);

SoftPWM servo9(PA_2);

SoftPWM servo10(PA_5);

SoftPWM servo11(PA_6);

SoftPWM servo12(PA_7);

SoftPWM servo13(PB_6);

SoftPWM servo14(PA_9);

SoftPWM servo15(PA_8);

SoftPWM servo16(PB_10);

SoftPWM servo17(PB_3);

SoftPWM servo18(PA_10);

int main() {

   servo1.period_us(20000);

   int servopulsewidth=1000;

   int si_mueve = 1200;

   int no_mueve = 1900;

   bool movimiento = false;

   servo1.pulsewidth_us(servopulsewidth);

   while(1){

     if (movimiento == true) {

      servo1.pulsewidth_us(si_mueve);

      serial.printf("YES: %f\r\n", servo1.read());

    } else {

      servo1.pulsewidth_us(no_mueve);

      serial.printf("NO: %f\r\n", servo1.read());

       

    }

     movimiento = !movimiento;

     wait_ms(250);

     }

}

This topic has been closed for replies.