Skip to main content
stst9184
Associate III
August 4, 2014
Question

Missing target STM32F411 in a Keil 5.11.1

Posted on August 04, 2014 at 10:28

How can I try the Nucleo board with a Keil. It reports a missing target ...411. Why that?

#keil #nucleo #stm32f411
This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
August 4, 2014
Posted on August 05, 2014 at 00:23

If you've installed all of the assorted packs and legacy stuff, your next stop should be support@keil.com

http://www.keil.com/support/contact.asp

http://www.keil.com/arm/chips.asp

Pretty sure you could pick a similar STM32F4 device and tweak the memory map, defines, etc and get it to compile.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
folsen
Visitor II
September 15, 2014
Posted on September 15, 2014 at 17:11

I am having a similar problem. Shouldn't this be in place before the product is released. Which micro is closest? STM32F407? F401? F415? 

Tesla DeLorean
Guru
September 15, 2014
Posted on September 15, 2014 at 18:21

I am having a similar problem. Shouldn't this be in place before the product is released.

I'm sure it is, have you spoken to your TOOL vendor? There's usually a patch or architecture file, and it would probably also be available to commercial ST clients through the normal support structures, ie reps and FAEs

The Nucleo board target mbed

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Nickname306_O
Visitor II
September 30, 2014
Posted on September 30, 2014 at 18:52

Hi joee,

if you are using an existing project, settings can not be lost and you will be able to compile/run it.

if you have created a new project, you can not select STM32F411 device since it is not yet supported.

Best Regards,

Nouha