Skip to main content
Victor Murilo Kostycha
Visitor II
Apr 29, 2022 3:12 PM UTC
Question

Migration STM32L151RTB6 to STM32L151RTB6A Backup register problem

Good morning!

I'm facing two kinds of problems, both when we are trying to boot the system by a remote application.

The first one is caused by a non writing of the RTC backup register. As shows the example below:

 0693W00000LzUf0QAF.jpg0693W00000LzUeHQAV.jpg 

As we can see, in the STM32L151RBT6A I can't write from the backup registers with address 0x40002864 forward, problem that doesn't happen in the STM32L151RBT6 Version. Following the datasheet, we can see that the new version has 20 thirty-two bits backup registers. There is any assumption why i can't use all of them? Just the first 5 ones and without change any configuration, the forward register is not writable? There is any division between the first 5 backup registers and the others 15?

The second one consists in a fail of flash, in the very first moment we receive the boot by GSM and we save the code in a external flash, the problem is that the micro seems to corrupt the external memory, it saves the code in the wrong address. This problem causes a total failure in our product. Using the same external flash with the micro RBT6 (not RBT6A) the problem doesn’t happen. Any idea what could be?

As I could verify in the datasheet, the differences between the 2 boards are usually related to the consumption of the board. This shouldn’t be a problem since my linear regulator is working with just 50% of his capacity.

I still haven’t found a solution for any of our problems.

I'm using the IAR Embedded workbench IDE, v8.32.4.

As compiler, the IAR standard compiler.

Thanks for your attention.

This topic has been closed for replies.