Skip to main content
AG1
Associate II
Oct 24, 2025 4:54 AM UTC
Question

Manual soldering profile details

Hi,

need information about the soldering profile for LQFP100 pin package in case, soldering the IC manually with temperature controlled soldering station

This topic has been closed for replies.

6 replies

AScha.3
Super User
Oct 24, 2025 7:03 AM UTC

Hi,

a soldering profile depends on the process for the used tin , not on the case of the parts.

So see the standard profile for your solder.

for RoHS, Pb free:

AScha3_0-1761289551550.pngAScha3_1-1761289586578.png

 

If you feel a post has answered your question, please click on " Best Answer ".
AG1
AG1Author
Associate II
Oct 24, 2025 11:38 AM UTC

Hi,

It seems max. temperature for soldering will be 260degC for manual process also on temperature controlled soldering station, then what could be temperature for de-soldering it?

as, during initial board bring up & trouble shooting , i would like to ensure that chip should not get damage during any process

AScha.3
Super User
Oct 24, 2025 12:47 PM UTC

Hi,

> temperature for de-soldering 

same as soldering, but maybe somewhat higher, because chip anyway going to trash then.

So its more : not damage the board. I use 350° (hot air) for desoldering, or hot plate at 260°.

The chips/parts usually not very sensitive to high temp. , if its just for short time.

https://www.ablic.com/en/semicon/support/package/solder-temp-profile/

 

For hand soldering typical recommendation is:  Resistance to soldering heat 260 °C/ 5 s  . (for relais here)

And as always: important is the flux , good flux.   And the way, you do it...experience helping a lot.

My preferred (and cheap) flux is NC-559 (see on Ali or ebay) , works fine with lead and lead free solder.

AScha3_0-1761309427702.png

https://youtu.be/rUmzN30lwP4

btw

I had already chips soldered and desoldered 2 times, chip still working fine. (at repairing boards with problems)

If you feel a post has answered your question, please click on " Best Answer ".
KDJEM.1
ST Technical Moderator
Oct 24, 2025 8:13 AM UTC

Hello @AG1 ;

 

I recommend you to look at Soldering recommendations and package information for lead-free ECOPACK2 MCUs and MPUs - Application note may help you.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
AG1
AG1Author
Associate II
Oct 24, 2025 11:39 AM UTC

thanks, already went through document, but unable to get the required info.

TDK
Oct 24, 2025 12:56 PM UTC

The chips are not particularly sensitive or delicate. Heat them up until the solder melts, hold a couple seconds, then let them cool down.

If you want the best reliability, use the recommended reflow profiles.

"If you feel a post has answered your question, please click ""Accept as Solution""."