Skip to main content
TLi.7
Associate
Mar 25, 2022 10:16 AM UTC
Question

M93C76RT self-timed programming cycle

Hi there,

From testing it's quite jarring to me to discover that after every 16bit write u need to wait ~5ms before the EEPROM will accept after write. After a more detail reading of the manual I found that after SPI write cmd the EEPROM will trigger a 'self-timed programming cycle' and it will last at least 4ms.

Want to make sure am I understanding this correctly? Or I am using it wrong? Also if this is the case what can it be used for?! I was originally to write diagnostic data to it periodically. But the 16 bit per 5ms speed is just way too low.

Thanks for reading, any reply is appreciated.

This topic has been closed for replies.

2 replies

Andreas Bolsch
Lead III
Mar 26, 2022 8:13 AM UTC

That's normal behaviour, not only for this type of EEPROM, but also for I2C-EEPROMs (m24xxx), SPI-EEPROMs (m25xxx) and SPI-Flash (but usually significantly less than 5ms).

However, except for the Microwire-EEPROMS (m93xxx) most higher densitity devices have a page write mode, where a block (16 bytes ... 256 bytes) can be written at once, i.e. the 5ms time covers the whole page write.

So, either take a device with large enough page size, or use several devices in parallel and use them interleaved or ... take an FRAM.

Another option would be an SPI-Flash, they have much shorter (page) programming time, but then the erase time comes into play. For a rotating log you'd have to use two in parallel, so you can write to one when on the other one a sector is being erased (or you need a sufficiently large RAM buffer).

TLi.7
TLi.7Author
Associate
Mar 27, 2022 6:50 AM UTC

Thanks a lot for the answer and advise!!!!! I never use any EEPROM chip before. I may need to consider to switch to one of those with page write function then. Anyway thanks again :folded_hands: