Skip to main content
Associate II
Feb 3, 2026 8:07 AM UTC
Question

Looking for help to integrate the external flash MX25L6433F

i am using nucleo-h753zi and i need to integrate external flash via spi, MX25L6433F this is my flash ic. i was struggling to integrate this flash so please guide me to achieve it also if possible please give any example code for this project

3 replies

Associate III
Feb 3, 2026 8:20 AM UTC

What do you want to achieve? Is it for dtaa storage or XIP?

Associate II
Feb 3, 2026 9:21 AM UTC

Hello Vidar,

Thank you for your response. Let me clarify what I'm trying to achieve:

        I want to integrate the external Macronix MX25L6433F SPI flash memory chip with my STM32H753ZI Nucleo board for data storage purposes (not XIP - Execute In Place).

What I want to do:
Read/Write/Erase data to the external flash memory.
Store application data, logs, or configuration parameters.
Basic flash memory operations (Read JEDEC ID, sector erase, page program, etc.).

Current Status:
Hardware: MX25L6433F flash chip connected via SPI1 (PA5=SCK, PA6=MISO, PA7=MOSI, PA4=CS).
I'm using STM32CubeIDE.
I'm trying to get basic SPI communication working to read the flash JEDEC ID.
Currently facing timeout issues with HAL_SPI_TransmitReceive.
Thank you.

mƎALLEm
ST Technical Moderator
Feb 3, 2026 8:32 AM UTC

Hello,

You may find MX25L6433F driver in X-CUBE-DISPLAY package.

Download the package and unzip it. You will find it under Drivers\BSP\Components\mx25l6433f

mALLEm_1-1770107519447.png

Or a ready to use external Flashloaders under the path \Utilities\PC_Software\ExternalLoader for the for specific ST boards if you are using one.

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.