Skip to main content
Visitor II
Jun 30, 2024 6:34 AM UTC
Question

Issue with Reading BMP280 Chip ID using SPI

Context: I am trying to read the Chip ID from a BMP280 sensor using SPI communication with an STM32 microcontroller. The expected Chip ID value is 0x58. However, I am encountering inconsistent results when calling the function to read the Chip ID multiple times.

 

BMP280_Read_CHIP_ID();
BMP280_Read_CHIP_ID();

 

Problem: When I call the BMP280_Read_CHIP_ID function twice consecutively, I get the following outputs:

  1. Chip ID Read - 0
  2. Chip ID Read - 58

00ef71ed-8c83-4ebc-9f56-f5dba0e7553b.png

UART Output.

The first read returns 0x00 (unexpected), while the second read returns the correct Chip ID 0x58.

Code:

Here is the function I am using to read the Chip ID:

 

 

void BMP280_Read_CHIP_ID()
{
 uint8_t data = 0;
 uint8_t address = 0xD0;
 address |= 0x80;
 CS_Enable();
 delay_ms(2);
 SPI_Transmit(&address, 1);
 delay_ms(2);
 SPI_Receive(&data, 1);
 delay_ms(2);
 CS_Disable();
 printf("Chip ID Read - %x\n\r", data);
}

 

 

SPI_Transmit Function:

 

void SPI_Transmit (uint8_t *data, int size)
{
	int i=0;
	while (i<size)
	{
	 while (!((SPI1->SR)&(1<<1))) {}; 
	 SPI1->DR = data[i]; 
	 i++;
	}

	while (!((SPI1->SR)&(1<<1))) {}; 
	while (((SPI1->SR)&(1<<7))) {}; 

	// Clear the Overrun flag by reading DR and SR
	uint8_t temp = SPI1->DR;
	temp = SPI1->SR;

}

 

SPI_Receive Function:

 

void SPI_Receive (uint8_t *data, int size)
{
	while (size)
	{
		while (((SPI1->SR)&(1<<7))) {};
		SPI1->DR = 0; // send dummy data
		while (!((SPI1->SR) &(1<<0))){}; 
	 *data++ = (SPI1->DR);
		size--;
	}
}

 

 

This topic has been closed for replies.

2 replies

Associate II
Jun 13, 2025 2:42 PM UTC

Hi @Kaarthy . You have probably already found a way to understand the issue. I am working on BMI323 shuttle board SPI communication between the nRF52840 DK, but I see the MOSI messages that I created, and the BMI323 is not returning anything MISO pin always shows 0x00. If possible, could you share your configuration code with me? Thanks for your response. 

Andrew Neil
Super User
Jun 13, 2025 2:51 PM UTC

Apart from the thread being a year old, and @Kaarthy having no activity at all on this forum since then, STM32 configuration code isn't going to help you on an nRF52840 DK !

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.