Skip to main content
Visitor II
Jul 7, 2025 12:34 PM UTC
Question

Issue with External Mode in Simulink when using ADC Injected Mode synchronized with PWM on STM32G4

Hello,
I’m working with Simulink and an STM32G4 series microcontroller. I’ve successfully set up PWM generation and configured the ADC in injected mode, synchronized with the PWM timer (TIM1).
However, when I enable External Mode in Simulink (for real-time parameter tuning and signal monitoring), the connection fails. Interestingly, everything works fine when I trigger the ADC using a different timer—the issue only occurs when TIM1 is used to trigger the injected ADC.
My setup:
  • Target: STM32G4 (e.g., STM32G4)
  • PWM generated using TIM1
  • ADC in injected mode, triggered by TIM1
  • External Mode communication over STLink (USB)
Question:
Is there a known limitation or conflict between External Mode and using injected ADC mode synchronized with PWM (via TIM1) on STM32 targets in Simulink?
Could this be related to timing/resource conflicts?
Do you have any suggestions or workarounds to maintain synchronized ADC injection while using External Mode?
Thanks in advance for your support!
This topic has been closed for replies.

1 reply

Andrew Neil
Super User
Jul 7, 2025 5:57 PM UTC

Simulink is a MathWorks product - nothing to do with ST - so you need to go to MathWorks for support:

https://uk.mathworks.com/help/?s_tid=nav_help_doc

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.