Skip to main content
Visitor II
May 14, 2025 6:11 PM UTC
Question

Issue using nRF24L01+ via SPI and STM32F0

I have a custom PCB using the STM32F042F. I replaced the STM, and now every time I connect the communication chip, the STM32 turns off. The STM does not boot if I first connect the nRF24L01 then power the STM.

 

I am confident my code and the board are not the issue, as it was functioning before I replaced the STM32 chip.

 

I think that some default configuration setting I am missing is causing the boards to short.

 

Does anyone have any ideas on how I can solve this issue?

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
May 23, 2025 10:40 AM UTC

Hello @JimJones12 and welcome to the community;

 

I think you have a hardware issue, ensure that the new STM32 is correctly replaced.

Check the power, ground connections and SPI communication lines. 

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.