Skip to main content
SElli.11
Associate III
Jul 15, 2019 3:01 PM UTC
Question

Is there any documentation that gives details of the C/C++ language that is used in Atollic TrueSTUDIO for STM32 v9.3.0? I'm looking for the names of keywords/commands as well as the signatures of functions.

I am very new to embedded systems programming. I have successfully installed Atollic TrueSTUDIO for STM32 v9.3.0 onto Kubuntu Linux 19.04. I want to use this IDE in conjunction with an STM32F407VGT Discovery board.

This topic has been closed for replies.

3 replies

Jack Peacock_2
Associate II
Jul 16, 2019 12:23 PM UTC

Just checked, v9.2.0 uses GCC v6.3.1 for the compiler. Search on GCC or GNU toolchain for the GCC documentation. There's a section in the GCC docs for ARM targets.

Jack Peacock

SElli.11
SElli.11Author
Associate III
Jul 17, 2019 10:17 AM UTC

Good morning Mr Peacock,

Thank you for your email. In line with your suggestion I've just completed a search for "gcc v6.3.1 documentation arm targets c lanuage reference" and found the following link.

https://gcc.gnu.org/onlinedocs/gcc-6.3.0/gcc.pdf

An examination of the contents page of this pdf does indeed contain reference to "3.18.4 ARM Options.......................................... 216". However, this lists compiler options which is necessary information although not the reference on the ARM C language that I was looking for. Still it is a good start so once again please accept my thanks for your help.

Yours sincerely,

Stuart Elliott

Piranha
Principal III
Jul 18, 2019 10:09 PM UTC