Skip to main content
m12lrpv
Associate III
Feb 13, 2021 9:45 AM UTC
Solved

Is there an updated eeprom emulation example for STM32F10x and CubeMX generated projects using HAL?

I've gone through AN2594 and the associated examples. They're all for the standard peripheral library which is now deprecated.

Someone has an example of a port on github that looks reasonably complete https://github.com/lamik/EEPROM-emulation-STM32F1-HAL/blob/master/Src/eeprom.c

and at this stage it looks like I will be using that

however...

I'm wondering it ST have (or are planning to have) an official update?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Feb 13, 2021 9:51 AM UTC

I thought they did, or had Cube auto-generate the boiler plate code.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Feb 13, 2021 9:51 AM UTC

I thought they did, or had Cube auto-generate the boiler plate code.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
m12lrpv
m12lrpvAuthor
Associate III
Feb 13, 2021 9:26 PM UTC

Thanks. Your suggestion regarding Cube generating the code sent me looking there.

I found that they ship examples in the CubeMX firmwares i.e. STM32Cube_FW_F1_V1.8.3

For the F4 firmware (STM32Cube_FW_F4_V1.25.2 ) the examples are selectable in the CubeMX example selector but not for the F1 examples.

:thumbs_up: